SWRU580 April 2021 CC2564C , CC2564MODA , CC2564MODN
This demo allows users to evaluate TI's CC256x Bluetooth device by using the Tiva DK-TM4C129X, MSP432 or STM32F4. The SPP sample application code is provided to enable a rich out-of-box experience to the user. The application allows the user to use a console to send Bluetooth commands, setup a Bluetooth Device to accept connections, connect to a remote Bluetooth device and communicate over Bluetooth. The Message Access Profile (MAP) sample application code is provided to enable a rich out-of-box experience to the user. The application allows the user to use a console to send Bluetooth commands, setup a Bluetooth Device to accept connections, connect to a remote Bluetooth device and communicate over Bluetooth.
It is recommended that the user visits the kit setup Getting Started Guide for MSP-430 or Getting Started Guide for TIVA pages before trying the application described on this page.Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as Tiva Virtual COM Port (COM x), XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud, 8, n, 1. Once connected, reset the device using Reset S3 button and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.
Figure 9-1 MAP Demo Initial Screen of PBAP Application