SWRU580 April 2021 CC2564C , CC2564MODA , CC2564MODN
This section provides a description of how to use the demo application to connect two configured board and communicate over Bluetooth. Bluetooth HFP is a simple Client-Server connection process with one side operating in the Audio-Gateway role and the other operating in the Handsfree role. We will setup one of the boards as a Handsfree server and use an android phone as Client. Once connected, we can transmit data between the two devices over Bluetooth
Server setup on the demo application
Figure 5-1 HFP Demo Start
Terminal
Figure 5-2 HFP Demo Set Local
Name
Figure 5-3 HFP Demo Open
Server
Figure 5-4 HFP Demo Discover
Device
Figure 5-5 HFP Demo Pair
Figure 5-7 HFP Demo Status
Indication Terminal
Figure 5-8 HFP Demo Manage Audio
Connection Terminal
Figure 5-9 HFP Demo Manage Audio
Connection Terminal 2
Figure 5-10 HFP Demo Answer Call
Terminal
Figure 5-11 HFP Demo Hang Up
Terminal
Figure 5-12 HFP Demo Close Server
Terminal