SBOSA39A April 2025 – October 2025 THS3470
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The IOUT_MONITOR pin is used to monitor the output current (IOUT) that is entering (sinking) or exiting (sourcing) the VOUT pin. To monitor the output current, the IOUT_MONITOR pin uses an internal current mirror to create a scaled-down current source that mirrors the output current through the VOUT pin. Equation 4 shows the equation that governs the relationship of the IOUT_MONITOR pin and output current.
For example, if the VOUT pin is sourcing 204.8mA, the IOUT_MONITOR pin sources 100µA. Alternatively, if the VOUT pin is sinking 204.8mA, the IOUT_MONITOR pin sinks 100µA.
To read the IOUT_MONITOR current with an ADC, include the external transimpedance circuit shown in Figure 6-6. This circuit is intended to achieve three key objectives. The first objective is to convert the IOUT_MONITOR pin current to a voltage (VOUT_TIA) that scales to match the ADC range (VADC_RANGE). The second objective is to shift the VOUT_TIA voltage to 1/2 VADC_RANGE when IOUT_MONITOR is equal to 0A. The last objective is to keep the IOUT_MONITOR pin within ±5V of the VMID voltage.
Resistor R1 in the transimpedance circuit is ultimately responsible for converting the maximum expected current (IMAX) from IOUT_MONITOR into a voltage that is optimized for the VADC_RANGE. To calculate R1 for the transimpedance circuit, use Equation 5.
For example, if the maximum expected current (typically governed by the output-current-limit pin configurations) is ±1A, the IMAX current is 1A / 2048 = 488µA. If a 3.3V ADC is used in the application, the VADC_RANGE for the application is 3.3V. Plugging these values into Equation 5 results in an R1 value of 3.381kΩ.
Resistor R2 in the transimpedance circuit is responsible for shifting VOUT_TIA to 1/2 of VADC_RANGE when IOUT_MONITOR is equal to 0A. To shift, use a proper reference voltage (VBIAS) that depends on the supply configuration of the THS3470. If the device is operating in a positive single-ended supply configuration (that is, VCC = 60V and VEE = 0V), then VBIAS can be connected to the VCC pin. If the device is operating in a negative single-ended supply configuration (that is, VCC = 0V and VEE = –60V), then VBIAS can be connected to the VEE pin. If the device is operating in a split-supply configuration (that is, VCC = 30V and VEE = –30V), then VBIAS can be connected to the ADC supply voltage (VADC). Ultimately, there is a large permutation of VBIAS voltages than can be used, but the suggested options are selected based on the available voltages already existing in the design. Equation 6 shows how to calculate R2 after the VBIAS voltage has been selected.
For example, if the R1 resistor is sized to convert a ±488µA current from IOUT_MONITOR to ±1.65V at VOUT_TIA, then the R2 resistor is selected to move the VOUT_TIA voltage to 1.65V (½ VADC_RANGE) when the IOUT_MONITOR current is 0A. The supply in this example is a split-supply configuration; therefore, VBIAS is tied to the ADC supply voltage VADC, which is 3.3V. The VMID voltage is always the average of VCC and VEE, resulting in a voltage of 0V for this example. Plugging in these values to Equation 6 results in an R2 value of 30kΩ.
The last resistor in the transimpedance amplifier circuit is R3, which is responsible for keeping the IOUT_MONITOR voltage within ±5V of the VMID voltage. R3 is also responsible for protecting the pin during start-up events for the THS3470, and is scaled to limit the input current to < 10mA. The noninverting input pin of the transimpedance amplifier is connected to VMID as well as the inverting input pin through negative feedback; therefore, R3 is sized to limit the voltage drop across R3 to ±4.5V. The maximum current that the THS3470 can provide is 2.1A at IOUT, which results in a maximum allowable current of approximately ±1mA from IOUT_MONITOR. Dividing the maximum allowable voltage of ±4.5V by the maximum current of ±1mA results in a resistance value of 4.5kΩ for R3.
After the components and bias voltages have been selected, Section 6.3.5 is used to convert VOUT_TIAvoltage read by the ADC to IOUT. In addition, Table 6-3 lists some common use cases to help select resistors and bias voltages.
| USE CASE | R2 (kΩ) | VBIAS (V) | V+ (V) | V– (V) |
|---|---|---|---|---|
| Split supply (±20V) | 40.96 | VEE | VADC | 0 |
| Split supply (±30V) | 61.44 | VEE | VADC | 0 |
| Single ended (40V) | 3.683 | VCC | VMID | 0 |
| Single ended (60V) | 3.576 | VCC | VMID | 0 |
| Single ended (–40V) | 3.121 | VEE | V | VMID |
| Single ended (–60V) | 3.203 | VEE | VADC | VMID |