SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
In the DCAN, the bit timing configuration is programmed in DCAN_BTR[14:0], additionally a baud rate prescaler extension of four bits (DCAN_BTR[19:16] BRPE) is provided.
Figure 24-178 Structure of the CAN Core’s CAN Protocol ControllerIn DCAN_BTR register, the components TSEG1, TSEG2, SJW and BRP have to be programmed to a numerical value that is one less than its functional value; so instead of values in the range of [1…n], values in the range of [0…n–1] are programmed. That way, e.g., SJW (functional range of [1…4]) is represented by only two bits.
Therefore, the length of the bit time is (programmed values) [TSEG1 + TSEG2 + 3] tq or (functional values) [Sync_Seg + Prop_Seg + Phase_Seg1 + Phase_Seg2] tq.
The data in the bit timing register (DCAN_BTR) is the configuration input of the CAN protocol controller. The baud rate prescaler (configured by BRPE/BRP) defines the length of the time quantum (the basic time unit of the bit time); the bit timing logic (configured by TSEG1, TSEG2, and SJW) defines the number of time quanta in the bit time.
The processing of the bit time, the calculation of the position of the sample point, and occasional synchronizations are controlled by the bit timing state machine, which is evaluated once each time quantum. The rest of the CAN protocol controller, the bit stream processor (BSP) state machine, is evaluated once each bit time, at the sample point.
The shift register serializes the messages to be sent and parallelizes received messages. Its loading and shifting is controlled by the BSP. The BSP translates messages into frames and vice versa. It generates and discards the enclosing fixed format bits, inserts and extracts stuff bits, calculates and checks the CRC code, performs the error management, and decides which type of synchronization is to be used. It is evaluated at the sample point and processes the sampled bus input bit. The time after the sample point that is needed to calculate the next bit to be sent (e.g., data bit, CRC bit, stuff bit, error flag, or idle) is called the information processing time (IPT), which is 0 tq for the DCAN.
Generally, the IPT is CAN controller-specific, but may not be longer than 2 tq. The IPC length is the lower limit of the programmed length of Phase_Seg2. In case of a synchronization, Phase_Seg2 may be shortened to a value less than IPT, which does not affect bus timing.