SBASAE3 December 2025 ADS125H18
PRODUCTION DATA
Figure 8-4 illustrates a 3-terminal, differential analog input module (AIM), using a discrete burden resistor for the 4-20mA measurement. In a typical 3-terminal input module, there is a separate screw terminal for each voltage and current input. During installation of the module, the user applies an external short between the V+ (voltage) and I+ (current) screw terminal, which eliminates the need for a switch selecting or deselecting the shunt resistor. Therefore, the overall measurement error for the current input is reduced, compared to the circuit which includes a select switch, as shown in Table 8-4.
Two ADC inputs are used per V/I differential input channel. Therefore, a maximum of 8 differential analog inputs can be implemented using one ADS125H18 device.