For all switching power supplies, the
layout is an important step in the design. If the layout is not carefully done, the
regulators can have stability and EMI issues. Therefore, use wide and short traces
for the main current path and for the power ground tracks. The input capacitors,
output capacitors, and inductors must be placed as close as possible to the device.
The output capacitors must have a low impedance to ground. Use multiple VIAS (at
least three) directly at the ground landing pad of the capacitor. Here are some
layout guidelines:
- PVIN_Bx: Place the input capacitor as
close to the IC as allowed by the layout DRC rules. Any extra parasitic
inductance between the input cap and the PVIN_Bx pin can create a voltage spike.
Use wide, short traces or polygon to help minimize trace inductance. Do not
route any sensitive signals close to the input cap and the device pin as this
node has high frequency switching currents. Add 3-4 vias per amp of current on
the GND pads for each DCDC. If there is limited space that does not allow for
the placement of the input capacitors on the same layer as the PMIC, then place
the input capacitors on the opposite layer with VIAS.
- LX_Bx: Place the inductor close to the
PMIC without compromising the PVIN input caps and use short and wide traces or
polygons to connect the pin to the inductor. Do not route any sensitive signals
close to this node. The inductor must be placed in the same layer as the IC to
prevent having to use VIAS in the SW node. The SW-node is the main generator of
EMI due to voltage swings from the input voltage to ground with very fast rise
and fall times. If needed, to reduce EMI, a RC snubber can be added to the SW
node.
- FB_Bx: Route each of the FB_Bx pins as a
trace to the output capacitor. Do not extend the output voltage polygon to the
FB_Bx pin as this pin requires to be routed as a trace. The trace resistance
from the output capacitor to the FB_Bx pin must be less than 1Ω. The TPS65214 does not support remote sensing so the
FB_Bx pins must be connected to the local capacitor of the PMIC. Avoid routing
the FB_Bx close to any noisy signals such as the switch node or under the
inductor to avoid coupling. If space is constraint, FB_Bx pin can be routed
through an inner layer. See example layout.
- Bucks Cout: The local output capacitors must be placed as close to the
inductor as possible to minimize electromagnetic emissions.
- VSYS/PVIN_LDO12: Place the input capacitor
as close as possible to the VSYS/PVIN_LDO12 pin. Route this input trace away
from PVIN_Bx to minimize noise coupling. If the space is limited and does not
allow placement of the input capacitors on the same layer as the PMIC, then
place the input capacitors on the opposite layer with VIAS, close to the
IC.
- VLDOx: Place the output capacitor close to
the VLDOx pin. For the LDO regulators, the feedback connection is internal.
Therefore, keep the PCB resistance between LDO output and target load in the
range of the acceptable voltage, IR, drop for LDOs.
- VDD1P8: Place the 2.2uF
cap as close as possible to the VDD1P8 pin. This capacitor needs to be placed in
the same layer as the IC. Two to Three VIAS can be used to connect the GND side
of the capacitor to the GND plane of the PCB.
- Power Pad: The thermal pad must be
connected to the PCB ground plane with a minimum of two VIAS.
- AGND: Do not connect AGND to the power pad
(or thermal pad). The AGND pin must be connected to the PCB ground planes
through a VIA. Keep the trace from the AGND pin to the VIA short.