SLVSHK7A March 2025 – December 2025 TPS65214
PRODUCTION DATA
When requesting a COLD reset, the device executes the power down sequence and transitions to INITIALIZE state. Then, the NVM is reloaded and rails power-up again in normal power-up-sequence, provided there are no faults and no OFF-request. A COLD reset returns all NVM-backed register bits to their boot-value. Register bits that are not NVM-backed maintain their values, except for STBY_I2C_CTRL, POWER_UP_FROM_OFF, POWER_UP_FROM_EN_PB_VSENSE, POWER_UP_FROM_FSD, CUST_PROG_DONE, CUST_NVM_VERIFY_DONE, and CUST_NVM_VERIFY_ERR. For details on which registers are NVM-backed, see Section 8.
The execution of a COLD-reset sets the bit COLD_RESET_ISSUED in POWER_UP_STATUS_REG register. The read-out of this bit allows the host to track if a COLD-reset was performed. The nINT-pin does not toggle based on this bit. Write W1C to clear the bit.
When requesting a WARM reset, all enabled rails remain on, but the output voltage of rails that support dynamic voltage change is reset to the boot-voltage. Specifically, following configurations get reset to their boot-value: BUCK1_VSET, BUCK2_VSET, BUCK3_VSET, LDO1_VSET, and LDO2_VSET. All other bits, even in the same register, remain at their current state. For example, LDOx_LSW_CONFIG, BUCKx_BW_SEL, BUCKx_UV_THR_SEL and the MFP_1_CONFIG register bits do NOT get reset during a WARM-reset.