SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Table 8-35 lists the memory-mapped registers for the CLA_REGS registers. All register offset addresses not listed in Table 8-35 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | MVECT1 | Task Interrupt Vector | EALLOW | Go |
| 1h | MVECT2 | Task Interrupt Vector | EALLOW | Go |
| 2h | MVECT3 | Task Interrupt Vector | EALLOW | Go |
| 3h | MVECT4 | Task Interrupt Vector | EALLOW | Go |
| 4h | MVECT5 | Task Interrupt Vector | EALLOW | Go |
| 5h | MVECT6 | Task Interrupt Vector | EALLOW | Go |
| 6h | MVECT7 | Task Interrupt Vector | EALLOW | Go |
| 7h | MVECT8 | Task Interrupt Vector | EALLOW | Go |
| 10h | MCTL | Control Register | EALLOW | Go |
| 1Bh | _MVECTBGRNDACTIVE | Active register for MVECTBGRND. | EALLOW | Go |
| 1Ch | SOFTINTEN | CLA Software Interrupt Enable Register | Go | |
| 1Dh | _MSTSBGRND | Status register for the back ground task. | EALLOW | Go |
| 1Eh | _MCTLBGRND | Control register for the back ground task. | EALLOW | Go |
| 1Fh | _MVECTBGRND | Vector for the back ground task. | EALLOW | Go |
| 20h | MIFR | Interrupt Flag Register | EALLOW | Go |
| 21h | MIOVF | Interrupt Overflow Flag Register | EALLOW | Go |
| 22h | MIFRC | Interrupt Force Register | EALLOW | Go |
| 23h | MICLR | Interrupt Flag Clear Register | EALLOW | Go |
| 24h | MICLROVF | Interrupt Overflow Flag Clear Register | EALLOW | Go |
| 25h | MIER | Interrupt Enable Register | EALLOW | Go |
| 26h | MIRUN | Interrupt Run Status Register | EALLOW | Go |
| 28h | _MPC | CLA Program Counter | Go | |
| 2Ah | _MAR0 | CLA Auxiliary Register 0 | Go | |
| 2Bh | _MAR1 | CLA Auxiliary Register 1 | Go | |
| 2Eh | _MSTF | CLA Floating-Point Status Register | Go | |
| 30h | _MR0 | CLA Floating-Point Result Register 0 | Go | |
| 34h | _MR1 | CLA Floating-Point Result Register 1 | Go | |
| 38h | _MR2 | CLA Floating-Point Result Register 2 | Go | |
| 3Ch | _MR3 | CLA Floating-Point Result Register 3 | Go | |
| 42h | _MPSACTL | CLA PSA Control Register | EALLOW | Go |
| 44h | _MPSA1 | CLA PSA1 Register | EALLOW | Go |
| 46h | _MPSA2 | CLA PSA2 Register | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 8-36 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W | W | Write |
| W1C | W 1C | Write 1 to clear |
| W1S | W 1S | Write 1 to set |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
MVECT1 is shown in Figure 8-10 and described in Table 8-37.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MVECT2 is shown in Figure 8-11 and described in Table 8-38.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MVECT3 is shown in Figure 8-12 and described in Table 8-39.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MVECT4 is shown in Figure 8-13 and described in Table 8-40.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MVECT5 is shown in Figure 8-14 and described in Table 8-41.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MVECT6 is shown in Figure 8-15 and described in Table 8-42.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MVECT7 is shown in Figure 8-16 and described in Table 8-43.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MVECT8 is shown in Figure 8-17 and described in Table 8-44.
Return to the Summary Table.
Each CLA interrupt has its own interrupt vector (MVECT1 to MVECT8). This interrupt vector points to the
first instruction of the associated task. When a task begins, the CLA will start fetching instructions at the
location indicated by the appropriate MVECT register .
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| MVECT | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MVECT | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | MVECT | R/W | 0h | MPC Start Address: These bits specify the start address for the given interrupt (task). The address range of the CLA with a 16-bit MVECT is 64Kx16 words or 32K CLA instructions. There is one MVECT register per interrupt (task). Interrupt 1 uses MVECT1, interrupt 2 uses MVECT2 and so forth. Note: While the CLA is running or executing a task, the CPU can change the MVECT values.. Reset type: SYSRSn |
MCTL is shown in Figure 8-18 and described in Table 8-45.
Return to the Summary Table.
Control Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | IACKE | SOFTRESET | HARDRESET | ||||
| R-0h | R/W-0h | R-0/W1S-0h | R-0/W1S-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-3 | RESERVED | R | 0h | Reserved |
| 2 | IACKE | R/W | 0h | IACK Operation Enable Bit: Writing a '1' to this bit will enable the IACK operation for setting the MIFR bits in the same manner as the MIFRC register (write of '1' will set respective MIFR bit). At reset, this feature is disabled. This feature enables the C28 CPU to efficiently trigger a task. Note: IACK operation should ignore EALLOW status of C28 core when accessing the MIFRC register. Reset type: SYSRSn 0h (R/W) = The CLA ignores the IACK instruction. (default) 1h (R/W) = Enable the main CPU to use the IACK #16bit instruction to set MIFR bits in the same manner as writing to the MIFRC register. Each bit in the operand, #16bit, corresponds to a bit in the MIFRC register. Using IACK has the advantage of not having to first set the EALLOW bit. This allows the main CPU to efficiently trigger a CLA task through software. Examples IACK #0x0001 Write a 1 to MIFRC bit 0 to force task 1 IACK #0x0003 Write a 1 to MIFRC bit 0 and 1 to force task 1 and task 2 |
| 1 | SOFTRESET | R-0/W1S | 0h | Soft Reset Bit: Writing a '1' to this bit will stop a current task, clear the RUN flag and also clear all bits in the MIER register. Writes of '0' are ignored and reads always return a '0'. Note: After issuing SOFTRESET command, user should wait at least 1 clock cycle before attempting to write to MIER register. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 are ignored. 1h (R/W) = Writing a 1 will cause a soft reset of the CLA. This will stop the current task, clear the MIRUN flag and clear all bits in the MIER register. After a soft reset you must wait at least 1 SYSCLKOUT cycle before reconfiguring the MIER bits. If these two operations are done back-to-back then the MIER bits will not get set. |
| 0 | HARDRESET | R-0/W1S | 0h | Hard Reset Bit: Writing a '1' to this bit will cause a HARD reset on the CLA. The behavior of a HARD reset is the same as a system reset SYSRSn on the CLA. Writes of '0' are ignored and reads always return a '0'. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 are ignored. 1h (R/W) = Writing a 1 will cause a hard reset of the CLA. This will set all CLA registers to their default state. |
_MVECTBGRNDACTIVE is shown in Figure 8-19 and described in Table 8-46.
Return to the Summary Table.
Gives the current interrupted MPC value of the background task, if the background task was running and interrupted, or reflects the MVECTBGRND value, if MCTLBGRND.BGSTART bit is 0.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| i16 | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i16 | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | i16 | R | 0h | Gives the current interrupted MPC value of the background task, if the background task was running and interrupted, or reflects the MVECTBGRND value, if MCTLBGRND.BGSTART bit is 0. Reset type: SYSRSn |
SOFTINTEN is shown in Figure 8-20 and described in Table 8-47.
Return to the Summary Table.
Enables the ability to generate CLA task interrupt from within the task, by writing to SOFTINTFRC register. SOFTINTFRC register can only be written from CLA. Only reads are allowed from CPU. Writes are not allowed from CPU.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| TASK8 | TASK7 | TASK6 | TASK5 | TASK4 | TASK3 | TASK2 | TASK1 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R/W | 0h | Reserved |
| 7 | TASK8 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
| 6 | TASK7 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
| 5 | TASK6 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
| 4 | TASK5 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
| 3 | TASK4 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
| 2 | TASK3 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
| 1 | TASK2 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
| 0 | TASK1 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
_MSTSBGRND is shown in Figure 8-21 and described in Table 8-48.
Return to the Summary Table.
Status bits for the backgrondtask.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | BGOVF | _BGINTM | RUN | ||||
| R/W-0h | R/W1C-0h | R-0h | R-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-3 | RESERVED | R/W | 0h | Reserved |
| 2 | BGOVF | R/W1C | 0h | Value of 1 indicates a hardware trigger (which is enabled) occurred while the MCTLBGRND.BGSTART bit is set. Writing a value of 1 to this bit clears the BGOVF bit. Write of 0 has no effect, Value of 0 indicates the background task trigger did not result in a overflow. Reset type: SYSRSn |
| 1 | _BGINTM | R | 0h | Value of 1 indicates that backgroiund task will not be interrupted. This bit is set when MSETC _BGINTM bit is executed. Value of 0 indicates that background task can be interrupted. Reset type: SYSRSn |
| 0 | RUN | R | 0h | Value of 1 indicates that background task is running. Value of 0 indicates that background task is not running. Reset type: SYSRSn |
_MCTLBGRND is shown in Figure 8-22 and described in Table 8-49.
Return to the Summary Table.
Holds the configuration bits to start the background task, enable hardware trigger.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| BGEN | RESERVED | ||||||
| R/W-0h | R/W-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TRIGEN | BGSTART | |||||
| R/W-0h | R/W-0h | R/W1S-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15 | BGEN | R/W | 0h | 0 Background task is disabled, BGSTART will not be set either in a hardware trigger or by writing 1 to BGSTART bit. 1 Background task is enabled and MIER[INT8] will be cleared, preventing task 8 from triggering. Reset type: SYSRSn |
| 14-2 | RESERVED | R/W | 0h | Reserved |
| 1 | TRIGEN | R/W | 0h | Hardware trigger enable for the background task. 1 Hardware trigger is enabled. 0 Hardware trigger is disabled. Note: Trigger source for the background task will be the same as that for task 8 Reset type: SYSRSn |
| 0 | BGSTART | R/W1S | 0h | Value of 1 will start the background task, provided there are no other pending tasks. - Value of 0 has no effect if the background task has not started. - This bit is also set by hardware, if MCTLBGRND.TRIGEN = 1 and a hardware trigger occurs. - This bit is cleared by hardware when a MSTOP instruction occurs in the background task - If the background task is running and this bit is cleared, it will not have any effect on the task execution. Reset type: SYSRSn |
_MVECTBGRND is shown in Figure 8-23 and described in Table 8-50.
Return to the Summary Table.
These bits specify the start address for the background task . The value in this register is forced into the MPC register when the background task starts.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| i16 | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i16 | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | i16 | R/W | 0h | MPC Start Address: These bits specify the start address for the background task . The value in this register is forced into the MPC register, when the background task starts. Reset type: SYSRSn |
MIFR is shown in Figure 8-24 and described in Table 8-51.
Return to the Summary Table.
Each bit in the interrupt flag register corresponds to a CLA task. The corresponding bit is automatically set
when the task request is received from the peripheral interrupt. The bit can also be set by the main CPU
writing to the MIFRC register or using the IACK instruction to start the task. To use the IACK instruction to
begin a task first enable this feature in the MCTL register. If the bit is already set when a new peripheral
interrupt is received, then the corresponding overflow bit will be set in the MIOVF register.
The corresponding MIFR bit is automatically cleared when the task begins execution. This will occur if the
interrupt is enabled in the MIER register and no other higher priority task is pending. The bits can also be
cleared manually by writing to the MICLR register. Writes to the MIFR register are ignored.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT8 | INT7 | INT6 | INT5 | INT4 | INT3 | INT2 | INT1 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | INT8 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 8 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 8 interrupt has been received and is pending execution |
| 6 | INT7 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 7 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 7 interrupt has been received and is pending execution |
| 5 | INT6 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 6 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 6 interrupt has been received and is pending execution |
| 4 | INT5 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 5 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 5 interrupt has been received and is pending execution |
| 3 | INT4 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 4 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 4 interrupt has been received and is pending execution |
| 2 | INT3 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 3 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 3 interrupt has been received and is pending execution |
| 1 | INT2 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 2 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 2 interrupt has been received and is pending execution |
| 0 | INT1 | R | 0h | These bits, when set to '1', indicate a valid peripheral interrupt has been latched by the CLA. Writes to this register are ignored. The IFR flag bit is automatically cleared if the respective interrupt is enabled in the MIER register and the respective task starts running. If a new peripheral interrupt attempts to set the bit to '1' while on the same cycle the task tries to clear it, then the peripheral interrupt will have priority. The IFR flag bits can also be set and cleared by the MIFRC and MICLR registers. If the MIFRC register is trying to set the respective bit while a new task tries to clear it, then the MIFRC event has priority. If the MICLR register is trying to clear the respective bit and a peripheral interrupt occurs on the same cycle, then the peripheral interrupt has priority. The respective overflow flag in the MIOVF register will not be set under this condition. Reset type: SYSRSn 0h (R/W) = TASK_FLAG_DISABLE Task 1 interrupt is currently not flagged (default) 1h (R/W) = TASK_FLAG_ENABLE Task 1 interrupt has been received and is pending execution |
MIOVF is shown in Figure 8-25 and described in Table 8-52.
Return to the Summary Table.
Each bit in the overflow flag register corresponds to a CLA task. The bit is set when an interrupt overflow
event has occurred for the specific task. An overflow event occurs when the MIFR register bit is already
set when a new interrupt is received from a peripheral source. The MIOVF bits are only affected by
peripheral interrupt events. They do not respond to a task request by the main CPU IACK instruction or by
directly setting MIFR bits. The overflow flag will remain latched and can only be cleared by writing to the
overflow flag clear (MICLROVF) register. Writes to the MIOVF register are ignored.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT8 | INT7 | INT6 | INT5 | INT4 | INT3 | INT2 | INT1 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | INT8 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 8 interrupt overflow has not occurred (default) 1h (R/W) = A task 8 interrupt overflow has occurred |
| 6 | INT7 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 7 interrupt overflow has not occurred (default) 1h (R/W) = A task 7 interrupt overflow has occurred |
| 5 | INT6 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 6 interrupt overflow has not occurred (default) 1h (R/W) = A task 6 interrupt overflow has occurred |
| 4 | INT5 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 5 interrupt overflow has not occurred (default) 1h (R/W) = A task 5 interrupt overflow has occurred |
| 3 | INT4 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 4 interrupt overflow has not occurred (default) 1h (R/W) = A task 4 interrupt overflow has occurred |
| 2 | INT3 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 3 interrupt overflow has not occurred (default) 1h (R/W) = A task 3 interrupt overflow has occurred |
| 1 | INT2 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 2 interrupt overflow has not occurred (default) 1h (R/W) = A task 2 interrupt overflow has occurred |
| 0 | INT1 | R | 0h | These bits, when set to '1', indicate an interrupt overflow event occurred. Such an event occurs when the IFR bit is already set. An overflow event remains latched and respective bits can only be cleared by writing to the MICLROVF register. If the MIFR bit is being cleared by a new task on the same cycle as a new peripheral interrupt occurs, the overflow flag will not be affected and the respective MIFR bit will be set. If the MIOVF bit is being cleared by the MICLROVF register on the same cycle as the overflow bit is being set by hardware, then the hardware will have priority. Notes: [1] The MIOVF bits are only affected by peripheral interrupt events. Forcing an interrupt using the MIFRC or IACK operation will not set the overflow flag even if the MIFR bit is set. Reset type: SYSRSn 0h (R/W) = A task 1 interrupt overflow has not occurred (default) 1h (R/W) = A task 1 interrupt overflow has occurred |
MIFRC is shown in Figure 8-26 and described in Table 8-53.
Return to the Summary Table.
The interrupt force register can be used by the main CPU to start tasks through software. Writing a 1 to a
MIFRC bit will set the corresponding bit in the MIFR register. Writes of 0 are ignored and reads always
return 0. The IACK #16bit operation can also be used to start tasks and has the same effect as the
MIFRC register. To enable IACK to set MIFR bits you must first set the MCTL[IACKE] bit. Using IACK has
the advantage of not having to first set the EALLOW bit. This allows the main CPU to efficiently trigger
CLA tasks through software.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT8 | INT7 | INT6 | INT5 | INT4 | INT3 | INT2 | INT1 |
| R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | INT8 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 8 interrupt |
| 6 | INT7 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 7 interrupt |
| 5 | INT6 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 6 interrupt |
| 4 | INT5 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 5 interrupt |
| 3 | INT4 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 4 interrupt |
| 2 | INT3 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 3 interrupt |
| 1 | INT2 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 2 interrupt |
| 0 | INT1 | R-0/W1S | 0h | Writing a '1' to any of the bits will set the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to force the task 1 interrupt |
MICLR is shown in Figure 8-27 and described in Table 8-54.
Return to the Summary Table.
Normally bits in the MIFR register are automatically cleared when a task begins. The interrupt flag clear
register can be used to instead manually clear bits in the interrupt flag (MIFR) register. Writing a 1 to a
MICLR bit will clear the corresponding bit in the MIFR register. Writes of 0 are ignored and reads always
return 0.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT8 | INT7 | INT6 | INT5 | INT4 | INT3 | INT2 | INT1 |
| R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | INT8 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 8 interrupt flag |
| 6 | INT7 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 7 interrupt flag |
| 5 | INT6 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 6 interrupt flag |
| 4 | INT5 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 5 interrupt flag |
| 3 | INT4 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 4 interrupt flag |
| 2 | INT3 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 3 interrupt flag |
| 1 | INT2 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 2 interrupt flag |
| 0 | INT1 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIFR bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIFR register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 1 interrupt flag |
MICLROVF is shown in Figure 8-28 and described in Table 8-55.
Return to the Summary Table.
Overflow flag bits in the MIOVF register are latched until manually cleared using the MICLROVF register.
Writing a 1 to a MICLROVF bit will clear the corresponding bit in the MIOVF register. Writes of 0 are
ignored and reads always return 0.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT8 | INT7 | INT6 | INT5 | INT4 | INT3 | INT2 | INT1 |
| R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | INT8 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 8 interrupt overflow flag |
| 6 | INT7 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 7 interrupt overflow flag |
| 5 | INT6 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 6 interrupt overflow flag |
| 4 | INT5 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 5 interrupt overflow flag |
| 3 | INT4 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 4 interrupt overflow flag |
| 2 | INT3 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 3 interrupt overflow flag |
| 1 | INT2 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 2 interrupt overflow flag |
| 0 | INT1 | R-0/W1S | 0h | Writing a '1' to any of the bits will clear the corresponding MIOVF bit. Writes of '0' are ignored. Reads always return 0. Notes: [1] Refer to MIOVF register description for handling of boundary conditions. Reset type: SYSRSn 0h (R/W) = This bit always reads back 0 and writes of 0 have no effect 1h (R/W) = Write a 1 to clear the task 1 interrupt overflow flag |
MIER is shown in Figure 8-29 and described in Table 8-56.
Return to the Summary Table.
Setting the bits in the interrupt enable register (MIER) allow an incoming interrupt or main CPU software to
start the corresponding CLA task. Writing a 0 will block the task, but the interrupt request will still be
latched in the flag register (MIFLG). Setting the MIER register bit to 0 while the corresponding task is
executing will have no effect on the task. The task will continue to run until it hits the MSTOP instruction.
When a soft reset is issued, the MIER bits are cleared. There should always be at least a 1 SYSCLKOUT
delay between issuing the soft reset and reconfiguring the MIER bits.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT8 | INT7 | INT6 | INT5 | INT4 | INT3 | INT2 | INT1 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | INT8 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 8 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 8 interrupt is enabled |
| 6 | INT7 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 7 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 7 interrupt is enabled |
| 5 | INT6 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 6 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 6 interrupt is enabled |
| 4 | INT5 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 5 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 5 interrupt is enabled |
| 3 | INT4 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 4 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 4 interrupt is enabled |
| 2 | INT3 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 3 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 3 interrupt is enabled |
| 1 | INT2 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 2 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 2 interrupt is enabled |
| 0 | INT1 | R/W | 0h | Setting any of the bits to '1' enables the corresponding interrupt from triggering a corresponding CLA task. Writing a '0' blocks the interrupt, but the interrupt can still be latched by the MIFR register. When an interrupt is enabled and the corresponding MIFR bit is set to '1', the CLA will start executing the corresponding task and automatically clear the corresponding MIFR bit. Interrupts are be serviced in normal priority order. Notes: [1] If a task is currently executing and the corresponding MIER bit is cleared to '0', it will have no effect on the task. The task will run until it hits the STOP instruction. Reset type: SYSRSn 0h (R/W) = TASK_INT_DISABLE Task 1 interrupt is disabled (default) 1h (R/W) = TASK_INT_ENABLE Task 1 interrupt is enabled |
MIRUN is shown in Figure 8-30 and described in Table 8-57.
Return to the Summary Table.
The interrupt run status register (MIRUN) indicates which task is currently executing. Only one MIRUN bit
will ever be set to a 1 at any given time. The bit is automatically cleared when the task competes and the
respective interrupt is fed to the peripheral interrupt expansion (PIE) block of the device. This lets the main
CPU know when a task has completed. The main CPU can stop a currently running task by writing to the
MCTL[SOFTRESET] bit. This will clear the MIRUN flag and stop the task. In this case no interrupt will be
generated to the PIE.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT8 | INT7 | INT6 | INT5 | INT4 | INT3 | INT2 | INT1 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | INT8 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 8 is not executing (default) 1h (R/W) = Task 8 is executing |
| 6 | INT7 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 7 is not executing (default) 1h (R/W) = Task 7 is executing |
| 5 | INT6 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 6 is not executing (default) 1h (R/W) = Task 6 is executing |
| 4 | INT5 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 5 is not executing (default) 1h (R/W) = Task 5 is executing |
| 3 | INT4 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 4 is not executing (default) 1h (R/W) = Task 4 is executing |
| 2 | INT3 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 3 is not executing (default) 1h (R/W) = Task 3 is executing |
| 1 | INT2 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 2 is not executing (default) 1h (R/W) = Task 2 is executing |
| 0 | INT1 | R | 0h | These bits indicate which task is currently active. Only one bit can be set to '1' at any one time. The bit is automatically cleared to '0' when the task completes and the respective CLAINTxn line is toggled to indicate task completion. The CLAINTxn interrupt line can be fed to the PIE of the CPU so the CPU knows when a task has completed. A currently running task can be stopped by a SOFTRESET. The RUN flag is cleared, the task is stopped, but no CLAINTxn interrupt is generated. Reset type: SYSRSn 0h (R/W) = Task 1 is not executing (default) 1h (R/W) = Task 1 is executing |
_MPC is shown in Figure 8-31 and described in Table 8-58.
Return to the Summary Table.
CLA Program Counter
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| _MPC | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| _MPC | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | _MPC | R | 0h | Program Counter: The PC value is initialized by the appropriate MVECTx register when an interrupt (task) is serviced. The MPC register address 16-bits and not 32-bits. Hence the address range of the CLA with a 16-bit MPC is 64Kx16 words or 32K CLA instructions. Notes: [1] To be consistent with C28 core implementation, the PC value points to the instruction in D2 stage of pipeline. [2] After a STOP operation, and with no other task pending, the PC will remain pointing to the STOP operation. Reset type: SYSRSn |
_MAR0 is shown in Figure 8-32 and described in Table 8-59.
Return to the Summary Table.
CLA Auxiliary Register 0
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| _MAR0 | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| _MAR0 | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | _MAR0 | R | 0h | CLA Auxillary Register 0 Reset type: SYSRSn |
_MAR1 is shown in Figure 8-33 and described in Table 8-60.
Return to the Summary Table.
CLA Auxiliary Register 1
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| _MAR1 | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| _MAR1 | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | _MAR1 | R | 0h | CLA Auxillary Register 1 Reset type: SYSRSn |
_MSTF is shown in Figure 8-34 and described in Table 8-61.
Return to the Summary Table.
The CLA status register (MSTF) reflects the results of different operations. These are the basic rules for
the flags:
- Zero and negative flags are cleared or set based on:
- floating-point moves to registers
- the result of compare, minimum, maximum, negative and absolute value operations
- the integer result of operations such as MMOV16, MAND32, MOR32, MXOR32, MCMP32,
MASR32, MLSR32
- Overflow and underflow flags are set by floating-point math instructions such as multiply, add, subtract
and 1/x. These flags may also be connected to the peripheral interrupt expansion (PIE) block on your
device. This can be useful for debugging underflow and overflow conditions within an application.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | _RPC | ||||||
| R-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| _RPC | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| _RPC | MEALLOW | RESERVED | RNDF32 | RESERVED | |||
| R-0h | R-0h | R-0h | R-0h | R-0h | |||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TF | RESERVED | ZF | NF | LUF | LVF | |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-28 | RESERVED | R | 0h | Reserved |
| 27-12 | _RPC | R | 0h | Return program counter The _RPC is used to save and restore the MPC address by the MCCNDD and MRCNDD operations Reset type: SYSRSn |
| 11 | MEALLOW | R | 0h | MEALLOW Status This bit enables and disables CLA write access to EALLOW protected registers This is independent of the state of the EALLOW bit in the main CPU status register This status bit can be saved and restored by the MMOV32 STF, mem32 instruction Reset type: SYSRSn 0h (R/W) = The CLA cannot write to EALLOW protected registers. This bit is cleared by the CLA instruction, MEDIS. 1h (R/W) = The CLA is allowed to write to EALLOW protected registers. This bit is set by the CLA instruction, MEALLOW. |
| 10 | RESERVED | R | 0h | Reserved |
| 9 | RNDF32 | R | 0h | Round 32-bit Floating-Point Mode Use the MSETFLG and MMOV32 MSTF, mem32 instructions to change the rounding mode Reset type: SYSRSn 0h (R/W) = If this bit is zero, the MMPYF32, MADDF32 and MSUBF32 instructions will round to zero (truncate). 1h (R/W) = If this bit is one, the MMPYF32, MADDF32 and MSUBF32 instructions will round to the nearest even value. |
| 8-7 | RESERVED | R | 0h | Reserved |
| 6 | TF | R | 0h | Test Flag The MTESTTF instruction can modify this flag based on the condition tested The MSETFLG and MMOV32 MSTF, mem32 instructions can also be used to modify this flag Reset type: SYSRSn 0h (R/W) = The condition tested with the MTESTTF instruction is false. 1h (R/W) = The condition tested with the MTESTTF instruction is true. |
| 5-4 | RESERVED | R | 0h | Reserved |
| 3 | ZF | R | 0h | Zero Flag - Instructions that modify this flag based on the floating-point value stored in the destination register: MMOV32, MMOVD32, MABSF32, MNEGF32 - Instructions that modify this flag based on the floating-point result of the operation: MCMPF32, MMAXF32, and MMINF32 - Instructions that modify this flag based on the integer result of the operation: MMOV16, MAND32, MOR32, MXOR32, MCMP32, MASR32, MLSR32 and MLSL32 The MSETFLG and MMOV32 MSTF, mem32 instructions can also be used to modify this flag Reset type: SYSRSn 0h (R/W) = The value is not zero 1h (R/W) = The value is zero |
| 2 | NF | R | 0h | Negative Flag - Instructions that modify this flag based on the floating-point value stored in the destination register: MMOV32, MMOVD32, MABSF32, MNEGF32 - Instructions that modify this flag based on the floating-point result of the operation: MCMPF32, MMAXF32, and MMINF32 - Instructions that modify this flag based on the integer result of the operation: MMOV16, MAND32, MOR32, MXOR32, MCMP32, MASR32, MLSR32 and MLSL32 The MSETFLG and MMOV32 MSTF, mem32 instructions can also be used to modify this flag Reset type: SYSRSn 0h (R/W) = The value is not negative 1h (R/W) = The value is negative |
| 1 | LUF | R | 0h | Latched Underflow Flag The following instructions will set this flag to 1 if an underflow occurs: MMPYF32, MADDF32, MSUBF32, MMACF32, MEINVF32, MEISQRTF32 The MSETFLG and MMOV32 MSTF, mem32 instructions can also be used to modify this flag Reset type: SYSRSn 0h (R/W) = An underflow condition has not been latched 1h (R/W) = An underflow condition has been latched |
| 0 | LVF | R | 0h | Latched Overflow Flag The following instructions will set this flag to 1 if an overflow occurs: MMPYF32, MADDF32, MSUBF32, MMACF32, MEINVF32, MEISQRTF32 The MSETFLG and MMOV32 MSTF, mem32 instructions can also be used to modify this flag Reset type: SYSRSn 0h (R/W) = An overflow condition has not been latched 1h (R/W) = An overflow condition has been latched |
_MR0 is shown in Figure 8-35 and described in Table 8-62.
Return to the Summary Table.
CLA Floating-Point Result Register 0
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i32 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | i32 | R | 0h | CLA Result Register 0 Reset type: SYSRSn |
_MR1 is shown in Figure 8-36 and described in Table 8-63.
Return to the Summary Table.
CLA Floating-Point Result Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i32 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | i32 | R | 0h | CLA Result Register 1 Reset type: SYSRSn |
_MR2 is shown in Figure 8-37 and described in Table 8-64.
Return to the Summary Table.
CLA Floating-Point Result Register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i32 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | i32 | R | 0h | CLA Result Register 2 Reset type: SYSRSn |
_MR3 is shown in Figure 8-38 and described in Table 8-65.
Return to the Summary Table.
CLA Floating-Point Result Register 3
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i32 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | i32 | R | 0h | CLA Result Register 3 Reset type: SYSRSn |
_MPSACTL is shown in Figure 8-39 and described in Table 8-66.
Return to the Summary Table.
PSA Control Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MPSA2CFG | MPSA2CLEAR | MPSA1CLEAR | MDWDBCYC | MDWDBSTART | MPABCYC | MPABSTART | |
| R/W-0h | R-0/W1S-0h | R-0/W1S-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | RESERVED | R | 0h | Reserved |
| 7-6 | MPSA2CFG | R/W | 0h | CLA PSA2 Polynomial Configuration Bits: These bits configure the type of polynomial used for PSA2. The polynomials chosen are commonly used in the industry: Mode Polynomial Type 0,0 PSA 0,1 CRC32 1,0 CRC16 1,1 CRC16-CCITT Note: [1] Polynomial configuration should be performed when PSA2 is stopped. Reset type: SYSRSn |
| 5 | MPSA2CLEAR | R-0/W1S | 0h | CLA PSA2 Clear Bit: Writing of '1' will clear contents of PSA2 register. Writes of '0' are ignored. Always reads back a '0' Note: Clearing operation should be performed when PSA2 is stopped. Reset type: SYSRSn |
| 4 | MPSA1CLEAR | R-0/W1S | 0h | CLA PSA1 Clear Bit: Writing of '1' will clear contents of PSA1 register. Writes of '0' are ignored. Always reads back a '0' Note: Clearing operation should be performed when PSA1 is stopped. Reset type: SYSRSn |
| 3 | MDWDBCYC | R/W | 0h | CLA Data Write Data Bus PSA2 Cycle or Event Based Bit: 0 PSA2 calculated on every cycle 1 PSA2 calculated on every bus event Reset type: SYSRSn |
| 2 | MDWDBSTART | R/W | 0h | CLA Data Write Data Bus PSA2 Start/Stop Bit: 0 PSA2 stopped 1 PSA2 start Reset type: SYSRSn |
| 1 | MPABCYC | R/W | 0h | CLA Program Address Bus PSA1 Cycle/Event Based Bit: 0 PSA1 calculated on every cycle 1 PSA1 calculated on every bus event Reset type: SYSRSn |
| 0 | MPABSTART | R/W | 0h | CLA Program Address Bus PSA1 Start/Stop Bit: 0 PSA1 stopped 1 PSA1 start Reset type: SYSRSn |
_MPSA1 is shown in Figure 8-40 and described in Table 8-67.
Return to the Summary Table.
PSA1 Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i32 | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | i32 | R/W | 0h | PSA1 Value: Reading this register gives the current PSA1 value. The value can be read at any time. Writes to this register are allowed to initialize the PSA1 to a known value. Writes to this register should only be made when PSA1 is stopped. Register value is cleared to zero by reset or by writing to the MPSA1CLEAR bit in the MPSACTL register. Reset type: SYSRSn |
_MPSA2 is shown in Figure 8-41 and described in Table 8-68.
Return to the Summary Table.
PSA2 Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| i32 | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | i32 | R/W | 0h | PSA2 Value: Reading this register gives the current PSA2 value. The value can be read at any time. Writes to this register are allowed to initialize the PSA2 to a known value. Writes to this register should only be made when PSA2 is stopped. Register value is cleared to zero by reset or by writing to the MPSA2CLEAR bit in the MPSACTL register. Reset type: SYSRSn |