SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The transmitter and receiver cores can be connected together internally to allow for development and debug. This is achieved by setting RX_MASTER_CTRL.INT_LOOPBACK to 1. Internal loopback routes the signals from the corresponding transmitter to the appropriate receiver pin. No configuration needs to be done in the transmitter. Figure 32-9 shows the signal connections with internal loopback.
In this device, there are two FSI transmitter cores (A and B), and eight receiver cores (A, B, C, D, E, F, G, and H). When using loopback mode, FSITXA can be used in the loopback mode with FSIRXA, FSIRXB, FSIRXC, and FSIRXD. At the same time, FSITXB can be used in loopback mode with FSIRXE, FSIRXF, FSIRXG, and FSIRXH.
Figure 32-9 FSI with Internal
Loopback