SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Table 20-87 lists the memory-mapped registers for the ADC_RESULT_REGS registers. All register offset addresses not listed in Table 20-87 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | ADCRESULT0 | ADC Result 0 Register | Go | |
| 1h | ADCRESULT1 | ADC Result 1 Register | Go | |
| 2h | ADCRESULT2 | ADC Result 2 Register | Go | |
| 3h | ADCRESULT3 | ADC Result 3 Register | Go | |
| 4h | ADCRESULT4 | ADC Result 4 Register | Go | |
| 5h | ADCRESULT5 | ADC Result 5 Register | Go | |
| 6h | ADCRESULT6 | ADC Result 6 Register | Go | |
| 7h | ADCRESULT7 | ADC Result 7 Register | Go | |
| 8h | ADCRESULT8 | ADC Result 8 Register | Go | |
| 9h | ADCRESULT9 | ADC Result 9 Register | Go | |
| Ah | ADCRESULT10 | ADC Result 10 Register | Go | |
| Bh | ADCRESULT11 | ADC Result 11 Register | Go | |
| Ch | ADCRESULT12 | ADC Result 12 Register | Go | |
| Dh | ADCRESULT13 | ADC Result 13 Register | Go | |
| Eh | ADCRESULT14 | ADC Result 14 Register | Go | |
| Fh | ADCRESULT15 | ADC Result 15 Register | Go | |
| 10h | ADCPPB1RESULT | ADC Post Processing Block 1 Result Register | Go | |
| 12h | ADCPPB2RESULT | ADC Post Processing Block 2 Result Register | Go | |
| 14h | ADCPPB3RESULT | ADC Post Processing Block 3 Result Register | Go | |
| 16h | ADCPPB4RESULT | ADC Post Processing Block 4 Result Register | Go |
Complex bit access types are encoded to fit into small table cells. Table 20-88 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
ADCRESULT0 is shown in Figure 20-97 and described in Table 20-89.
Return to the Summary Table.
ADC Result 0 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 0 16-bit ADC result. After the ADC completes a conversion of SOC0, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT1 is shown in Figure 20-98 and described in Table 20-90.
Return to the Summary Table.
ADC Result 1 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 1 16-bit ADC result. After the ADC completes a conversion of SOC1, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT2 is shown in Figure 20-99 and described in Table 20-91.
Return to the Summary Table.
ADC Result 2 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 2 16-bit ADC result. After the ADC completes a conversion of SOC2, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT3 is shown in Figure 20-100 and described in Table 20-92.
Return to the Summary Table.
ADC Result 3 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 3 16-bit ADC result. After the ADC completes a conversion of SOC3, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT4 is shown in Figure 20-101 and described in Table 20-93.
Return to the Summary Table.
ADC Result 4 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 4 16-bit ADC result. After the ADC completes a conversion of SOC4, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT5 is shown in Figure 20-102 and described in Table 20-94.
Return to the Summary Table.
ADC Result 5 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 5 16-bit ADC result. After the ADC completes a conversion of SOC5, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT6 is shown in Figure 20-103 and described in Table 20-95.
Return to the Summary Table.
ADC Result 6 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 6 16-bit ADC result. After the ADC completes a conversion of SOC6, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT7 is shown in Figure 20-104 and described in Table 20-96.
Return to the Summary Table.
ADC Result 7 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 7 16-bit ADC result. After the ADC completes a conversion of SOC7, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT8 is shown in Figure 20-105 and described in Table 20-97.
Return to the Summary Table.
ADC Result 8 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 8 16-bit ADC result. After the ADC completes a conversion of SOC8, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT9 is shown in Figure 20-106 and described in Table 20-98.
Return to the Summary Table.
ADC Result 9 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 9 16-bit ADC result. After the ADC completes a conversion of SOC9, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT10 is shown in Figure 20-107 and described in Table 20-99.
Return to the Summary Table.
ADC Result 10 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 10 16-bit ADC result. After the ADC completes a conversion of SOC10, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT11 is shown in Figure 20-108 and described in Table 20-100.
Return to the Summary Table.
ADC Result 11 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 11 16-bit ADC result. After the ADC completes a conversion of SOC11, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT12 is shown in Figure 20-109 and described in Table 20-101.
Return to the Summary Table.
ADC Result 12 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 12 16-bit ADC result. After the ADC completes a conversion of SOC12, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT13 is shown in Figure 20-110 and described in Table 20-102.
Return to the Summary Table.
ADC Result 13 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 13 16-bit ADC result. After the ADC completes a conversion of SOC13, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT14 is shown in Figure 20-111 and described in Table 20-103.
Return to the Summary Table.
ADC Result 14 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 14 16-bit ADC result. After the ADC completes a conversion of SOC14, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCRESULT15 is shown in Figure 20-112 and described in Table 20-104.
Return to the Summary Table.
ADC Result 15 Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESULT | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESULT | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | RESULT | R | 0h | ADC Result 15 16-bit ADC result. After the ADC completes a conversion of SOC15, the digital result is placed in this bit field. Reset type: SYSRSn |
ADCPPB1RESULT is shown in Figure 20-113 and described in Table 20-105.
Return to the Summary Table.
ADC Post Processing Block 1 Result Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SIGN | PPBRESULT | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | SIGN | R | 0h | Sign Extended Bits. These bits reflect the same value as bit 16. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the SIGN bits extend down to bit 12, and all reflect the same value as bit 12. Reset type: SYSRSn |
| 15-0 | PPBRESULT | R | 0h | ADC Post Processing Block Result 1 The result of the offset/reference subtraction post conversion processing is stored in this register. This result is available 1 SYSCLK cycle after the associated ADCRESULT is available. If ADCINTFLG is polled to determine when to read the PPBRESULT, it may be necessary to add a NOP instruction to ensure that the updated post conversion processing result has posted to the register. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the PPBRESULT bits are limited to bits 12:0. Reset type: SYSRSn |
ADCPPB2RESULT is shown in Figure 20-114 and described in Table 20-106.
Return to the Summary Table.
ADC Post Processing Block 2 Result Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SIGN | PPBRESULT | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | SIGN | R | 0h | Sign Extended Bits. These bits reflect the same value as bit 16. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the SIGN bits extend down to bit 12, and all reflect the same value as bit 12. Reset type: SYSRSn |
| 15-0 | PPBRESULT | R | 0h | ADC Post Processing Block Result 2 The result of the offset/reference subtraction post conversion processing is stored in this register. This result is available 1 SYSCLK cycle after the associated ADCRESULT is available. If ADCINTFLG is polled to determine when to read the PPBRESULT, it may be necessary to add a NOP instruction to ensure that the updated post conversion processing result has posted to the register. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the PPBRESULT bits are limited to bits 12:0. Reset type: SYSRSn |
ADCPPB3RESULT is shown in Figure 20-115 and described in Table 20-107.
Return to the Summary Table.
ADC Post Processing Block 3 Result Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SIGN | PPBRESULT | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | SIGN | R | 0h | Sign Extended Bits. These bits reflect the same value as bit 16. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the SIGN bits extend down to bit 12, and all reflect the same value as bit 12. Reset type: SYSRSn |
| 15-0 | PPBRESULT | R | 0h | ADC Post Processing Block Result 3 The result of the offset/reference subtraction post conversion processing is stored in this register. This result is available 1 SYSCLK cycle after the associated ADCRESULT is available. If ADCINTFLG is polled to determine when to read the PPBRESULT, it may be necessary to add a NOP instruction to ensure that the updated post conversion processing result has posted to the register. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the PPBRESULT bits are limited to bits 12:0. Reset type: SYSRSn |
ADCPPB4RESULT is shown in Figure 20-116 and described in Table 20-108.
Return to the Summary Table.
ADC Post Processing Block 4 Result Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SIGN | PPBRESULT | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | SIGN | R | 0h | Sign Extended Bits. These bits reflect the same value as bit 16. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the SIGN bits extend down to bit 12, and all reflect the same value as bit 12. Reset type: SYSRSn |
| 15-0 | PPBRESULT | R | 0h | ADC Post Processing Block Result 4 The result of the offset/reference subtraction post conversion processing is stored in this register. This result is available 1 SYSCLK cycle after the associated ADCRESULT is available. If ADCINTFLG is polled to determine when to read the PPBRESULT, it may be necessary to add a NOP instruction to ensure that the updated post conversion processing result has posted to the register. NOTE: If the conversion associated with this Post Processing Block is a 12-bit conversion, the PPBRESULT bits are limited to bits 12:0. Reset type: SYSRSn |