The F28E12x devices
provide some methods to reduce the device current consumption:
- One of
the two low-power modes—IDLE or STANDBY—could be
entered during idle periods in the application.
- The flash
module may be powered down if the code is run from
RAM.
- Disable
the pullups on pins that assume an output
function.
- To
realize the lowest VDDA current consumption in an
LPM, see the Analog-to-Digital Converter (ADC)
chapter of the F28E12x
Real-Time Microcontrollers Technical Reference
Manual to ensure each module is powered
down as well.