SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The cipher feedback (CFB) mode is similar to the output feedback (OFB) mode, with the key difference being that the input block to the block cipher E used to generate the key stream is taken from the previous ciphertext block (after being XORed with the plaintext), vs. taken before being XORed with the plaintext (as in the case of OFB). As a result, the keystream is dependent upon the plaintext, which is not true of OFB. The CFB cipher is shown in Figure 10-5.
Like OFB, CFB requires an initialization vector (IV). In CFB mode, the initialization vector (IV) must be unpredictable.
The AESADV accelerator supports automated CFB mode operation of more than 128 bits of data either through interrupts or through the use of DMA. Software interrupt-based multi-block handling uses the AES interrupt condition reported in the CPU_INT.IIDX.STAT field. If this field reads 0x2 (INPUTRDY), then the next block of input can be written (as 4 32-bit writes). If this field reads 0x1 (OUTPUTRDY), then the output block can be read (as 4 32-bit reads).
In DMA mode, CFB utilizes two DMA channels. Channel bound to DMA_TRIG_DATAIN is the input channel. Channel bound to DMA_TRIG_DATAOUT is the output channel. The channels need to be configured to perform one 32-bit read/write per trigger.