SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
In 8-mux mode, each segment pin drives eight LCD segments, and eight common lines (COM0 through COM7) are used. Figure 20-7 shows some example 8-mux 1/3-bias waveforms.
Figure 20-7 Example
8-Mux, 1/3 Bias Waveforms (LCDLP = 0)Figure 20-8 shows some example 8-mux 1/3-bias waveforms with LCDLP = 1. With LCDLP = 1, the voltage sequence compared to the non-low power waveform is reshuffled; that is, all of the timeslots marked with "*" in Figure 20-7 are grouped together. The same principle applies to all mux modes.
Figure 20-8 Example
8-Mux, 1/3 Bias Low-Power Waveforms (LCDLP = 1)