SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The RTC is configured with the RTC peripheral registers. There are two ways of resetting the RTC state depending on whether a device includes the Low-Frequency Sub System (LFSS).
The RTC state can be reset at any time through one of these two methods:
The RTC is configured with the RTC peripheral registers. In RTC instance only, the RTC must be enabled before being configured for use by setting the ENABLE bit in the PWREN register (see peripheral power enable) together with the matching PWREN KEY value. RTC_x instances do not need a power enable register.
Application software may reset the RTC state at any time by setting the RESETASSERT bit in the RSTCTL register of the RTC together with the matching RSTCTL KEY value. The RESETSTKY bit in the STAT register of the RTC will be set following a reset of the RTC. This flag may be cleared by setting the RESETSTKYCLR bit in the RSTCTL register of the RTC. As such, software may determine if the RTC has been reset since the sticky reset bit (RESETSTKY) was last cleared. Many RTC registers have no initial conditions. These registers must be configured by application software before use.
To start the RTC counters, the MODCLKEN bit in the CLKCTL register must be set by application software. The MODCLKEN bit is initially cleared following a reset of the RTC.
When enabled and configured, the RTC runs in all power modes except SHUTDOWN. The RTC is not reset by a CPURST, SYSRST, or NRST pin triggered BOOTRST (see the reset control section for a detailed overview of device reset levels). As such, the RTC continues to operate even through software invocation of the bootstrap loader (BSL) or a hold of <1s on the external NRST pin.