SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The AES module provides a trigger source which can be configured to source DMA trigger 1. The DMA1 trigger events from the AES are given in Table 30-469. When the DMA1 channel is needed by the AES for block cipher operations, the DMA1 trigger should be unmasked in the IMASK register of DMA_TRIG_DATAOUT and the DMA should be configured as needed to support the AES operation.
| Index (IIDX) | Name | Description |
|---|---|---|
| 0 | NO_INTR | No DMA Trig1 Event Pending |
| 1 | TRIG1 | DMA Trigger for Data Output |
The DMA trigger 1 event configuration is managed with the DMA_TRIG_DATAOUT event management registers. See Section 7.2.5 for guidance on configuring the event registers for DMA triggers.