SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The wake up controller (WUC) is responsible for monitoring for assertion of interrupts when the processor is powered down in the STOP or STANDBY operating mode. In these modes, the entire PD1 power domain is power gated, and as such, the processor and NVIC are not available to check for interrupts. The WUC retains a copy of which peripheral interrupt sources to the NVIC were enabled when the processor entered STOP or STANDBY mode. In the event that an enabled interrupt is issued, the WUC will handshake with the PMCU to bring the device out of STOP or STANDBY mode so that the CPU can service the interrupt. The WUC will capture the interrupt state and present it to the NVIC and processor when the processor is brought up, such that the processor will see the interrupt even if the raw interrupt status of the peripheral is removed before the processor finishes powering up to service the interrupt.
The WUC requires no configuration by application software upon entry to or exit from low-power modes, and operation is transparent to application software.