SPRAD05E August 2024 – October 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
Refer On-Chip Debug chapter of device-specific TRM for supported debug functionalities.
Refer below sections of the of the On-Chip Debug chapter:
Emulation control inputs EMU0 and EMU1 are used to configure the debug boot mode behavior. Emulation control inputs EMU0 and EMU1 can be used to enable the boundary scan test capability.
Debug Boot Mode
Emulation control inputs EMU0 and EMU1 are sampled when MCU_PORz input is deasserted and the decoded value determines the debug boot mode behavior as detailed in Table Debug Boot Modes of the On-Chip Debug chapter of device-specific TRM.
Boundary Scan Compliance
Emulation control inputs EMU0 and EMU1 are sampled when TRSTn is deasserted and the decoded value determines the debug boot mode behavior as detailed in Table Boundary Scan Compliance of the On-Chip Debug chapter of device-specific TRM.
Debug or boundary scan functionalities does not have any dependency on boot mode configuration.