SBAA178A March 2011 – November 2026 ADS1286 , ADS7223 , ADS7229 , ADS7230 , ADS7263 , ADS7279 , ADS7280 , ADS774 , ADS7800 , ADS7812 , ADS7813 , ADS7815 , ADS7816 , ADS7817 , ADS7818 , ADS7822 , ADS7822-Q1 , ADS7823 , ADS7824 , ADS7825 , ADS7826 , ADS7827 , ADS7828 , ADS7828-Q1 , ADS7829 , ADS7830 , ADS7834 , ADS7835 , ADS7841 , ADS7841-Q1 , ADS7842 , ADS7844 , ADS7852 , ADS7861 , ADS7862 , ADS7863 , ADS7864 , ADS7865 , ADS7866 , ADS7867 , ADS7868 , ADS7869 , ADS7870 , ADS7871 , ADS7881 , ADS7882 , ADS7883 , ADS7884 , ADS7885 , ADS7886 , ADS7887 , ADS7888 , ADS7890 , ADS7891 , ADS7924 , ADS7945 , ADS7946 , ADS7947 , ADS7948 , ADS7949 , ADS7950 , ADS7951 , ADS7952 , ADS7953 , ADS7954 , ADS7955 , ADS7956 , ADS7957 , ADS7958 , ADS7959 , ADS7960 , ADS7961 , ADS8201 , ADS8284 , ADS8317 , ADS8318 , ADS8319 , ADS8320 , ADS8320-HT , ADS8321 , ADS8322 , ADS8323 , ADS8324 , ADS8325 , ADS8326 , ADS8327 , ADS8328 , ADS8329 , ADS8330 , ADS8331 , ADS8332 , ADS8341 , ADS8342 , ADS8344 , ADS8345 , ADS8361 , ADS8363 , ADS8364 , ADS8365 , ADS8370 , ADS8371 , ADS8372 , ADS8380 , ADS8381 , ADS8382 , ADS8383 , ADS8405 , ADS8406 , ADS8411 , ADS8412 , ADS8413 , ADS8422 , ADS8471 , ADS8472 , ADS8481 , ADS8482 , ADS8484 , ADS8504 , ADS8505 , ADS8506 , ADS8507 , ADS8508 , ADS8509 , ADS8512 , ADS8513 , ADS8515 , ADS8517 , ADS8519 , ADS8528 , ADS8548 , ADS8555 , ADS8556 , ADS8557 , ADS8558 , ADS8568 , ADS8634 , ADS8638 , TLC0820A , TLC0831 , TLC0832 , TLC0834 , TLC0838 , TLC1514 , TLC1518 , TLC1542 , TLC1543 , TLC1543-EP , TLC1549 , TLC1550 , TLC1551 , TLC2543 , TLC2543-EP , TLC2543-Q1 , TLC2543M , TLC2551 , TLC2552 , TLC2554 , TLC2555 , TLC2558 , TLC2574 , TLC2578 , TLC3541 , TLC3544 , TLC3545 , TLC3548 , TLC3574 , TLC3578 , TLC4541 , TLC4545 , TLV0831 , TLV0832 , TLV0834 , TLV0838 , TLV1504 , TLV1508 , TLV1543 , TLV1544 , TLV1548 , TLV1548-EP , TLV1548-Q1 , TLV1548M , TLV1549 , TLV1570 , TLV1571 , TLV1572 , TLV1578 , TLV2541 , TLV2542 , TLV2543 , TLV2544 , TLV2544Q , TLV2545 , TLV2548 , TLV2548-EP , TLV2548M , TLV2548Q , TLV2553 , TLV2553-Q1 , TLV2556 , TLV2556-EP , TLV571
This report analyzes the input structure along with the driving circuit of a SAR ADC. It provides a simple analytical method for calculating minimum acquisition times for SAR ADCs when a constant dc voltage is applied to the input. Three different test cases were calculated using exact equations as well as simplified ones. The difference in the final acquired voltage calculated with these two equations was negligible. Last of all, it was shown through calculations and test cases that the minimum acquisition time of a system with constant dc source will be less than the identical system using an input step function (see Reference 1).