SBAA178A March 2011 – November 2026 ADS1286 , ADS7223 , ADS7229 , ADS7230 , ADS7263 , ADS7279 , ADS7280 , ADS774 , ADS7800 , ADS7812 , ADS7813 , ADS7815 , ADS7816 , ADS7817 , ADS7818 , ADS7822 , ADS7822-Q1 , ADS7823 , ADS7824 , ADS7825 , ADS7826 , ADS7827 , ADS7828 , ADS7828-Q1 , ADS7829 , ADS7830 , ADS7834 , ADS7835 , ADS7841 , ADS7841-Q1 , ADS7842 , ADS7844 , ADS7852 , ADS7861 , ADS7862 , ADS7863 , ADS7864 , ADS7865 , ADS7866 , ADS7867 , ADS7868 , ADS7869 , ADS7870 , ADS7871 , ADS7881 , ADS7882 , ADS7883 , ADS7884 , ADS7885 , ADS7886 , ADS7887 , ADS7888 , ADS7890 , ADS7891 , ADS7924 , ADS7945 , ADS7946 , ADS7947 , ADS7948 , ADS7949 , ADS7950 , ADS7951 , ADS7952 , ADS7953 , ADS7954 , ADS7955 , ADS7956 , ADS7957 , ADS7958 , ADS7959 , ADS7960 , ADS7961 , ADS8201 , ADS8284 , ADS8317 , ADS8318 , ADS8319 , ADS8320 , ADS8320-HT , ADS8321 , ADS8322 , ADS8323 , ADS8324 , ADS8325 , ADS8326 , ADS8327 , ADS8328 , ADS8329 , ADS8330 , ADS8331 , ADS8332 , ADS8341 , ADS8342 , ADS8344 , ADS8345 , ADS8361 , ADS8363 , ADS8364 , ADS8365 , ADS8370 , ADS8371 , ADS8372 , ADS8380 , ADS8381 , ADS8382 , ADS8383 , ADS8405 , ADS8406 , ADS8411 , ADS8412 , ADS8413 , ADS8422 , ADS8471 , ADS8472 , ADS8481 , ADS8482 , ADS8484 , ADS8504 , ADS8505 , ADS8506 , ADS8507 , ADS8508 , ADS8509 , ADS8512 , ADS8513 , ADS8515 , ADS8517 , ADS8519 , ADS8528 , ADS8548 , ADS8555 , ADS8556 , ADS8557 , ADS8558 , ADS8568 , ADS8634 , ADS8638 , TLC0820A , TLC0831 , TLC0832 , TLC0834 , TLC0838 , TLC1514 , TLC1518 , TLC1542 , TLC1543 , TLC1543-EP , TLC1549 , TLC1550 , TLC1551 , TLC2543 , TLC2543-EP , TLC2543-Q1 , TLC2543M , TLC2551 , TLC2552 , TLC2554 , TLC2555 , TLC2558 , TLC2574 , TLC2578 , TLC3541 , TLC3544 , TLC3545 , TLC3548 , TLC3574 , TLC3578 , TLC4541 , TLC4545 , TLV0831 , TLV0832 , TLV0834 , TLV0838 , TLV1504 , TLV1508 , TLV1543 , TLV1544 , TLV1548 , TLV1548-EP , TLV1548-Q1 , TLV1548M , TLV1549 , TLV1570 , TLV1571 , TLV1572 , TLV1578 , TLV2541 , TLV2542 , TLV2543 , TLV2544 , TLV2544Q , TLV2545 , TLV2548 , TLV2548-EP , TLV2548M , TLV2548Q , TLV2553 , TLV2553-Q1 , TLV2556 , TLV2556-EP , TLV571
In order to evaluate if the approximation derived in Equation 12 is valid, the following test cases were analyzed for a 16-bit ADC (N = 16):
The results of these cases are displayed in Table 5-1.
| Parameter | Case | Units | ||
|---|---|---|---|---|
| (a) | (b) | (c) | ||
| R1 | 100 | 100 | 10 | Ω |
| C1 | 1000 | 1000 | 100 | pF |
| R2 | 20 | 2000 | 2000 | Ω |
| C2 | 50 | 50 | 50 | pF |
![]() | 1.59 | 1.59 | 159 | MHz |
![]() | 159 | 1.59 | 1.59 | MHz |
| f2/f1 | 100 | 1 | 0.01 | |
| a(1) | 100 | 100 | 1 | ns |
| b(1) | 5 | 5 | 0.5 | ns |
| c(1) | 1 | 100 | 100 | ns |
| ωn(1) | 100 | 10 | 100 | Mrad/s |
(1) | 5.300 | 1.025 | 5.075 | |
![]() | 105.048 | 125.000 | 100.505 | ns |
![]() | 0.952 | 80.000 | 0.995 | ns |
| tACQ | 0.920 | 1.399 | 1.184 | μs |
| k1(tACQ) | 0.000008 | 0.000008 | 0.000008 | |
| k2(tACQ) | 0.000000 | 0.000000 | 0.000000 | |
| A(tACQ)EQ08
(Equation 9) | 0.999992 | 0.999992 | 0.999992 | |
| A(tACQ)EQ11 (Equation 12) | 0.999992 | 0.999992 | 0.999992 | |
| Error(2) | 0.000000 | 0.000001 | 0.000000 | % |

By using the acquisition times from Table 5-1, the final voltage on the sampling capacitor of the ADC from Figure 2-1 was calculated for each test case by using Equation 12 and Equation 9. The difference in the final voltage calculated with Equation 12 and Equation 9 for each test case is negligible (see Table 5-1 for details). This analysis clearly demonstrates that using the simplified Equation 12 to calculate the final voltage on the sampling capacitor does not introduce any significant error compared to using the exact formula (Equation 9). This assessment is further supported by the plots in Figure 5-1 through Figure 5-3. Another insight revealed by this analysis is that the acquisition times in Table 5-1 are less than the corresponding ones in the previous application report (see Reference 1).
Figure 5-1 Case (a)
Figure 5-3 Case (c)
Figure 5-2 Case (b)