SLLSFO8C May 2024 – November 2025 TCAN2450-Q1 , TCAN2451-Q1
PRODUCTION DATA
VSUP is the primary input supply rail required for the device to function properly. There are three voltage levels monitored by the device-power on reset and two under-voltage levels. For all functions and output voltage rails to be in regulation, the VSUP rail must exceed UVSUP5R. If VSUP is in under-voltage, the device loses the supply source needed to keep the internal regulators in regulation. If VSUP keeps ramping down and drops below VSUP(PU)F, the device enters powered off state. When VSUP returns, the device comes up as if the initial power is on. All registers are cleared and the device has to be reconfigured from the stored EEPROM values that were retained. Please see the power brown-out diagrams Figure 10-3, Figure 10-4, Figure 10-6, and Figure 10-6 for further information.
When VCC1 is configured for 5V output, UVSUP5R/F is the only VSUP under-voltage rail monitored. When VSUP drops below UVSUP5F, The CAN transceiver is turned off and the device enters a protected UVSUP state. VCC2 LDO is in pass thru mode and can trigger UVCC2 event. The VCC1 regulator is in a maximum duty cycle switching mode and can trigger a UVCC1 event depending upon the chosen UVCC1 threshold. See Table 8-14 for relationship between VSUP, VCC15, VCAN, device mode and the CAN transceiver.
When VCC1 is configured for 3.3V output, both UVSUP33R/F and UVSUP5R/F are monitored. When powering up, VSUP has to exceed UVSUP33R for VCC1 to be in regulation and above UVSUP5R for VCC2 and other functions of the device to work properly. When VSUP is ramping down, UVSUP5F is the first UVSUP level that sets an UVSUP5 interrupt flag, register 8’h52[4], and turns off the CAN transceiver. If VSUP keeps dropping, the next level is UVSUP33F. When this is reached, the UVSUP33 interrupt flag is set, register 8’h52[3] and the device enters UVSUP mode. See Table 8-15 for relationship between VSUP, VCC133, VCAN, device mode and the CAN transceiver.
Under-voltage on the high-side switches power, VHSS, is indicated by interrupt INT_4 register 8'5A[0] UVHSS. The behavior of high-side switches due to an UVHSS event is determined by HSS_CNTL3 register 8'h4F[6:5].
| VSUP | VCC1 | VCAN | DEVICE STATE | CAN TRANSCEIVER |
|---|---|---|---|---|
| > UVSUP5 | > UVCC15 | > UVCAN | Normal or Standby | As Programmed |
| > UVSUP5 | < UVCC15 | N/A | Restart | Wake capable or off |
| > UVSUP5 | > UVCC15 | > UVCAN | Previous State | As Programmed |
| < UVSUP5 | > N/A | N/A | UVSUP | Off |
| > UVSUP5 | < UVCC15 | < UVCAN | Restart | Listen Mode |
| VSUP | VCC1 | VCAN | DEVICE STATE | CAN TRANSCEIVER |
|---|---|---|---|---|
| > UVSUP5 | > UVCC133 | > UVCAN | Normal or Standby | As Programmed |
| > UVSUP5 | < UVCC133 | N/A | Restart | Wake capable or off |
| > UVSUP5 | > UVCC133 | > UVCAN | Previous State | As Programmed |
| < UVSUP5 > UVSUP33 | > UVCC133 | N/A | Normal or Standby | Off |
| < UVSUP5 > UVSUP33 | < UVCC133 | N/A | Restart | Off |
| < UVSUP33 | N/A | N/A | UVSUP | Off |
| > UVSUP5 | > UVCC133 | < UVCAN | Normal or Standby | Wake capable or off |