SLUUB65B May 2015 – December 2022
This read-only command pair returns the modified full charge capacity based on the SOC smoothing algorithm. The value is modified during battery charge and is increased or decreased to achieve SOC convergence by the time end of charge is reached. For reporting of the capacity that can be extracted from a fully charged battery, the host should always refer to UnfilteredFCC(). Units are mAh. FilteredFCC() is updated at regular intervals, as specified by the IT algorithm.