A proper ChemID or profile for a given battery must be determined for the Impedance Track algorithm.
To determine ChemID for a given battery, do the following:
- Look up the cell/pack in the TI database to see if there is an existing ChemID already available. To do this, use BQStudio (http://www.ti.com/tool/BQStudio) with the latest chemistry plugin (http://www.ti.com/lit/zip/sluc564).
- If an existing ChemID cannot be found, use the Gauging Parameter Calculator Chemistry matching tool (GPCCHEM) to submit logs and get a closely matched ChemID. For more details, see the Simple Guide to Chemical ID Selection Tool (GPC) Application Note (SLVA725).
- If there is no match from either (1) or (2), cells can be sent to TI to characterize and generate a custom ChemID.