SLUUB65B May 2015 – December 2022
The AtRate() is a read-write function that reads or sets the load value used in computing load-compensated capacity in the Impedance Track algorithm when Load Mode = 0 or 1 and Load Select = 5. For configurations employing Load Mode = 0, the AtRate() register expects the host to write values in terms of mA. With a Load Mode of 1, the fuel gauge will expect units of mWh or cWh, depending on the setting for Design Energy Scale. The AtRate() value is a signed integer, with negative values interpreted as a discharge current value.