SLVAE87B December 2020 – June 2025 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
AVDD, CVDD, and DVDD are regulated outputs derived from the LDOIN input. Each of these regulator outputs have a bypass capacitor to avoid noise with a 10% tolerance due to the fact that a larger capacitance slows startup. REFHP is an internal reference voltage and NEG5V is a regulated voltage provided by an internal charge pump.
Each regulator provides power for delicate internal subsystems. Do not connect external circuitry or additional loads to these regulators beyond those described in the BQ79616-Q1, BQ79616H-Q1, BQ79614-Q1, BQ79612-Q1 Functional Safety-Compliant Automotive 16S/14S/12S Battery Monitor, Balancer and Integrated Hardware Protector data sheet.
Place the bypass capacitors of the following pins as close to the device pins as possible to make sure of proper performance, especially the REFHP capacitor. TI recommends to help performance with derating and emissions performance to utilize a small capacitor in parallel with each bypass LDO capacitor of 10-22%. For example, on CVDD, TI recommends both 22nF and 100nF capacitors in parallel with 4.7μF decoupling capacitor to help reduce emissions. These need to be designed extremely close to the pins of the IC in the layout for best effect.