SLVAE87B December 2020 – June 2025 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
One use of GPIO [7:4] is as a SPI master. Connection of the pins in SPI mode is the same as general digital connections, but SPI configuration replaces the GPIO pin configuration. Figure 7-2 shows an example connection of GPIO[7:4] for digital signaling or SPI mode.
Figure 7-2 Example SPI Master ConnectionsTie unused GPIO pins to AVSS through a 10kΩ pulldown resistor. By default, the GPIO pins are configured internally as an input with a weak pulldown resistor, so program the GPIO configuration appropriately to avoid leakage current.