SLVAE87B December 2020 – June 2025 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
During normal operation, a host can send a WAKE or SLEEPtoACTIVE ping to the base device and the corresponding tone is generated to the rest of the stack devices as seen in Figure 8-5. During system development, if there is a need to send WAKE or SLEEPtoACTIVE to only some of the devices in the daisy chain, then the host can use the CONTROL1[SEND_WAKE] or CONTROL1[SEND_SLPTOACT] bits. The SHUTDOWN and HW_RESET ping or tone are mostly used as a communication recovery attempt. Hence these pings/tones are non-propagable.
Figure 8-5 Diagram for Ping or Tone
Propagation