SLVAE87B December 2020 – June 2025 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
Place the bypass capacitors of the following pins as close to the device pins as possible to make sure of proper performance, especially the REFHP capacitor. TI recommends to help performance with derating and emissions performance to utilize a small capacitor in parallel with each bypass LDO capacitor of 10-22%. For example, on CVDD, TI recommends both a 22nF and 100nF capacitors in parallel with 4.7μF decoupling capacitor to help reduce emissions. These need to be designed extremely close to the pins of the IC in the layout for best effect.