SLVAE87B December 2020 – June 2025 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
Voltage monitoring is done through the VCn pins while cell balancing is done through the CBn pins. Each of the VCn pins is measured by the main SAR ADC to make sure of the most accurate readings. Getting an accurate reading for these connections is critical to achieve maximum performance so adhere to the following design recommendations.