SLVSHO1A March 2025 – December 2025 TPS1689
PRODUCTION DATA
POWER_CYCLE is a manufacturer specific command used to power down the output and power ON after a delay. The delay can be configured using the RETRY_CONFIG register. Execution of this command initiates a Power Path reset. The device state and register contents remain unchanged. Additionally, the command activates the QOD (Quick Output Discharge) mechanism to discharge the output load. The device verifies that the output is fully discharged before resuming normal operation.
This command uses the PMBus® send byte protocol. There is no data byte for this command. This command is write only.
This command should be preceded by the MFR_WRITE_PROTECT command to unlock the device first to prevent accidental/spurious writes. If the WP# pin is pulled low, the write access is completely disabled in hardware and MFR_WRITE_PROTECT command has no effect.
If the device is turned OFF due a fault, issuing a POWER_CYCLE command alone doesn't alter the state of the device. This command should be preceded by a CLEAR_FAULTS command.