| 31-17 | Reserved | 0 | Reads return 0. Writes have no effect. |
| 16 | CMPE2 | | Compare Error for VIM Output Compare Diagnostic. |
| Read in User and Privileged mode. Write in Privileged mode only. |
| 0 | Read: CPU signals are identical. |
| Write: Leaves the bit unchanged. |
| 1 | Read: CPU signal compare mismatch. |
| Write: Clears the bit. |
| 15-9 | Reserved | | Reads return 0. Writes have no effect. |
| 8 | STC2 | | Self-test Complete for VIM Output Compare Diagnostic. |
| Note: This bit is always 0 when not in self-test mode. Once set, switching from self-test mode to other modes will clear this bit. |
| Read/Write in User and Privileged mode. |
| 0 | Read: Self-test on-going if self-test mode is entered. |
| Write: Writes have no effect. |
| 1 | Read: Self-test is complete. |
| Write: Writes have no effect. |
| 7-2 | Reserved | | Reads return 0. Writes have no effect. |
| 1 | STET2 | | Self-test Error Type for VIM Output Compare Diagnostic. |
| Read/Write in User and Privileged mode. |
| 0 | Read: Self-test failed during Compare Match Test if STE2 = 1. |
| Write: Writes have no effect. |
| 1 | Read: Self-test failed during Compare Mismatch Test if STE2 = 1. |
| Write: Writes have no effect. |
| 0 | STE2 | | Self-test Error for VIM Output Compare Diagnostic. |
| Note: This bit gets updated when the self-test is complete or an error is detected. |
| Read/Write in User and Privileged mode. |
| 0 | Read: Self-test passed. |
| Write: Writes have no effect. |
| 1 | Read: Self-test failed. |
| Write: Writes have no effect. |