SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
eCAP modules can be synchronized with each other by selecting a common SYNCIN source. SYNCIN source for eCAP can be either software sync-in or external sync-in. The external sync-in signal can come from ePWM. The SWSYNC of the eCAP module is logical ORed with the SYNC signal as shown in Figure 7-251. The SYNC signal is defined by the selection of ECAPxSYNCINSEL[SEL] as shown in Figure 7-252.
Figure 7-251 Details of the Counter and
Synchronization Block