SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The following direct command status bits/registers are only set when error is generated and only cleared when the clear bit is written:
As these registers are reset only when the clear register is written, it is not possible to detect the falling edge on them to generate interrupts. Only the rising edges can generate the interrupt.
Note: There can be issues with detection when using the bits for all the signals that are a pulse generated in the tx_byte_hs_clk domain. When the speed of that clock is slower in relation to dsi_p_clk, it is possible to have the interrupt set, the bit read and the clear attempted before the end of the tx_byte_hs_clk pulse, after the clear, the bit is set again.