SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
A STIG request will cause the OSPI Flash controller to interrogate the OSPI_FLASH_CMD_CTRL_REG register to determine what and how many bytes it should send to the FLASH device. The OSPI_FLASH_CMD_CTRL_REG[31-24] CMD_OPCODE_FLD field of this register indicate the instruction to be sent and is always pushed first. If there is an address to send, then the address (the size of which is also programmed in the same register) is sent next. The address itself is stored in the OSPI_FLASH_CMD_ADDR_REG register. If Mode bits are enabled by OSPI_FLASH_CMD_CTRL_REG[18] ENB_MODE_BIT_FLD bit. OSPI_MODE_BIT_CONFIG_REG[7-0] MODE_FLD bit field are being sent right after address. If OSPI_FLASH_CMD_CTRL_REG[18] ENB_MODE_BIT_FLD and OSPI_CONFIG_REG[29] CRC_ENABLE_FLD are both enabled, STIG will replace XIP Mode bits (not applicable for CRC aware SPI interface) for automatically calculated address CRC byte. Therefore, to execute CRC aware STIGs (meaning the commands requiring sending address CRC byte), ENB_MODE_BIT_FLD bit should always be set. If there are any dummy cycles to send (the size of which is also programmed in OSPI_FLASH_CMD_CTRL_REG register) then those are sent next. If there is data to write or read (the size of which is also programmed in OSPI_FLASH_CMD_CTRL_REG register) then for the case of writes, up to 8 bytes can be sent (as stored in the Flash Command Write Data registers, OSPI_FLASH_WR_DATA_LOWER_REG and OSPI_FLASH_WR_DATA_UPPER_REG registers) next. In the read case, when the read data has been collected from the FLASH device, the OSPI Flash Controller stores that in the Flash Command Read Data Registers (OSPI_FLASH_RD_DATA_LOWER_REG and OSPI_FLASH_RD_DATA_UPPER_REG registers). Up to 8 bytes can be get if OSPI_FLASH_CMD_CTRL_REG[2] STIG_MEM_BANK_EN_FLD bit is disabled or up to 512 when enabled. When the OSPI Flash controller starts to service a STIG request, it sets the OSPI_FLASH_CMD_CTRL_REG[1] CMD_EXEC_STATUS_FLD bit to indicate a command execution is in progress. When the OSPI Flash controller is in the auto-polling state, servicing a STIG request is slightly different. Most of devices are largely inaccessible after a program operation until the device has completed that write. Some group of them has a possibility to suspend programming page. It can be controlled by the OSPI_POLLING_FLASH_STATUS_REG[8] DEVICE_STATUS_VALID_FLD bit, which indicate active auto-polling phase. After requesting a STIG, the OSPI Flash Controller immediately issues appropriate OPCODE to Memory. During servicing a STIG (in auto-polling phase) the status bit of command execution remains steady and other parts of transfer such as ADDRESS or DUMMY BITS, and so forth, are disabled (to issued Program Suspend Command is needed OPCODE only). There is a programmable option to add delay between every repetitive poll operation (delay is defined by OSPI_WRITE_COMPLETION_CTRL_REG[31-24] POLL_REP_DELAY_FLD bit field). This feature is implemented to free up SPI bandwidth if needed.
The OSPI data is sent LSB first, while address is sent MSB first.
The STIG complete status bit gets cleared before the actual flash access completes. Software should wait for about 700 ns if there is any dependency on actual access completion.