SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The Transaction Error Interrupt signals that the gasket has detected an error on a transaction. The gasket will return an appropriate response to the source side, so the source will not immediately violate a safety goal, but it is assumed that something uncorrected has happened in the system. The system must treat this as a dangerous event and react accordingly. The specific response is up to the system integrator, but possibilities are discussed below. There are three possible causes of the Transaction Error Interrupt, transaction timeout, unexpected response, and command timeout. Software should query the Error Interrupt Enabled Status/Clear Register (Base Address + 0x24) to determine the cause.