SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
Figure 12-195 Error Report and RecoveryFigure 1-1 shows concept of error report and its recovery. The Host Controller has 2 interrupt status registers. If an error occurs in the SD Bus transaction, one of the bits is set in the MMCSD0_ERROR_INTR_STS register. If the function errors occur in the SDIO card, the card interrupt informs these function errors and the Card interrupt is set in the MMCSD0_NORMAL_INTR_STS_ENA register (the Card Interrupt is used to inform not only error statuses but also normal information. For example, to inform function ready). The Card Driver shall do function error recovery because the Host Driver does not know how to control the function. In the case that function error occurs due to SD Bus error, SD Bus error recovery is required before function error recovery. Abort command is used to recover SD Bus, and then the Host Driver should save error statuses related to SD Bus errors before issuing abort command and transfer these statuses to the Card Driver. These statuses may be used to recover function error. Following explanations are related to SD Bus error recovery. This specification does not specify the function error recovery.
When an error occurs during data transfer in 2L-HD UHS-II mode, there will be the case that Host Controller cannot drive D0 lane in input mode due to DIR LSS for retrieving lane direction is not detected. In this case, Host Driver cannot issue abort command for recovery. Then if DIR LSS is not detected, Host Controller sets MMCSD0_UHS2_ERR_INTR_STS[17] DEADLOCK_TIMEOUT bit. Host Driver should execute power cycle if MMCSD0_UHS2_ERR_INTR_STS[17] DEADLOCK_TIMEOUT bit is detected to recover from this error. Furthermore, if this type of error is detected several times in 2L-HD, Host Driver should use FD mode rather than using 2L-HD.
Implementation Note:
If the Card Driver cannot recover the function errors, the Host Driver should try following methods.
(9) Using IOEx for SDIO card
IOEx may be used as the reset per function basis. Sequence is as follows:
Clear IOEx = 0 and wait until IORx = 0 and then set IOEx = 1 again. SDIO may be recovered when IORx = 1.
(10) Using reset command for memory and SDIO card Re-initialization sequence is required.
(11) Off and on power supply for the SD Bus.
The card may be recovered by the power on reset. Re-initialization sequence is required.
The two cases where the Host Driver needs the "Error Recovery" sequence are classified as follows:
(1) Error Interrupt Recovery:
If error interrupt is indicated by the MMCSD0_ERROR_INTR_STS register, the Host Driver shall apply this sequence.
(2) Auto CMD12 Error Recovery:
If there are errors in Auto CMD12, the Host Driver shall apply this sequence. In terms of Return Status, Auto CMD12 Error Recovery is classified into 4 cases. It is shown in Figure 12-196. If error occurs during memory write transfer, strongly recommend using ACMD22 and then in the following recovery sequence, retry to send remaining blocks not written.
Figure 12-196 Return Status of Auto CMD12 Error RecoveryImplementation Note:
Abort command is used to recover from SD Bus error. SDIO transaction abort using CMD52 returns response but in the case of memory transaction abort using CMD12, response returns depending on the memory card state. If no response returns after issue CMD12, the Host Driver should check card state using CMD13. If the state is "tran" in the CURRENT_STATE, consider CMD12 is successful.
Implementation Note:
The following sequence is one possible error recovery flow. There may be another methods, sometimes using interrupts or polling. It can be possible to use another flows, based on Host System requirements.
In these error recovery sequences, return statuses for the next sequence. When the Host Controller cannot issue the next command due to SD Bus error, the error recovery sequences return "Non-recoverable" status. In this case, the Host System may cut off power to the SD Bus and then power on SD Bus and initialize both the Host Controller and the SD card again.