SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The transmit data ready flag - XDATA in the MCASP_XSTAT register reflects the data ready status of XRBUFn buffers for all of the active slot transmitting serializers. The XDATA flag is set whenever data is transferred from a transmitting serializer buffer - XRBUFn to its corresponding XRSRn shift register. Thus, the XDATA bit indicates the global event that some of the serializers data buffer - XRBUFn is emptied and ready to accept new data from the host (CPU or DMA). The transmit data ready event is individually indicated per serializer in its corresponding control register MCASP_SRCTLn[4] XRDY status bit. When this bit is set to 0b1, it notifies to host that this serializer Tx buffer must be serviced (written). When MCASP_XBUFn is written to by the host, the MCASP_SRCTLn[4] XRDY is deasserted to 0b0. As XDATA global flag is an OR-event of all active serializers XRDY flags, it indicates to software the moment, when write service operation has to be initiated by the MCASP host (XDATA=0b1). The XRDY flags have to be sequentially scanned by user software to determine which serializer MCASP_XBUFn register has to be currently written. Once all requested MCASP_XBUFn are written, the serializers control XRDY flags are cleared to 0b0. As a consequence, XDATA flag is deasserted to 0b0, to indicate to SW that write operation is completed for all serializers.
The global XDATA flag can be cleared when the MCASP_XSTAT[5] XDATA bit is written to 0b1, or once MCASP_XBUFn registers of all the serializers, that have previously raised their XRDY flags, are written with corresponding active slot data by the host.
Whenever XDATA is set, the XINT event is automatically generated on MCASP[0-2]_XMIT_DMA_EVT line (if enabled in the MCASP_XEVTCTL register) to notify the DMA of the MCASP_XBUFn empty status. An interrupt - MCASP[0-2]_XMIT_INTR_PEND can be also generated if the XDATA interrupt is enabled in the MCASP_XINTCTL register (for details, see Section 12.5.2.3.13.1, Transmit Data Ready Interrupt).
For DMA requests, the MCASP does not require that MCASP_XSTAT register be read between DMA events. This means that, even if MCASP_XSTAT register already has the XDATA flag set to 1 from a previous request, the next transfer triggers another DMA request.
Because the serializer acts in lockstep, only one DMA event is generated to indicate that the transmit serializer is ready to be written to with new data.
Figure 12-347 shows the timing details of when XINT is generated at the MCASP boundary. In this example, as soon as the last bit (A0) of word A is transmitted, the MCASP sets the XDATA flag and generates an XINT event. However, it takes up to five MCASP interface clocks (XINT latency) before XINT is active at the MCASP boundary. Upon XINT, the CPU can begin servicing the MCASP by writing word C into the MCASP_XBUFn (service time). The CPU must write word C into the MCASP_XBUFn within the setup time required by the MCASP (setup time) (n = 0 to 15).
The maximum service time (see Figure 12-347) can be calculated as:
Service Time = Time Slot – XINT Latency –Setup Time
Figure 12-347 Service Time Upon Transmit DMA Event (XINT)