SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The DSI protocol states that, in the sending path, only the HS transmission requires use of EoT packet. For transfer from display to host, it is not recommended to use EoT but it is possible. The host needs to be able to detect the EoT packet and then behaves accordingly.
In case the display makes use of the EoT packet, the bit disp_eot_gen must be set to one. In that case, if after the ECC correction, the packet header is 0x08, we've detected an EoT packet and all bytes that may arrive between this packet and the direction change must be ignored.
If additional data is received between the EOT packet and the next BTA (end of read process), or if an unwanted EOT packet is detected, the unwanted bytes must be rejected and err_receive is asserted.
If the EoT packet is not detected although it should be present, the error err_missing_eot is set. If after an "acknowledge with error", 4 bytes are received before BTA but are not identified as EoT (because of errors), it is assumed these 4 bytes are the EoT. In that case, the error err_eot_with_err has to be set with err_undecodable.