SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Under normal conditions, only one controller device generates the clock signal, SCL. During the arbitration procedure, however, there are two or more controllers and the clock must be synchronized so that the data output can be compared. Figure 25-14 illustrates the clock synchronization. The wired-AND property of SCL means that a device that first generates a low period on SCL overrules the other devices. At this high-to-low transition, the clock generators of the other devices are forced to start a low period. The SCL is held low by the device with the longest low period. The other devices that finish the low periods must wait for SCL to be released, before starting the high periods. A synchronized signal on SCL is obtained, where the slowest device determines the length of the low period and the fastest device determines the length of the high period.
If a device pulls down the clock line for a longer time, the result is that all clock generators must enter the wait state. In this way, a target slows down a fast controller and the slow device creates enough time to store a received byte or to prepare a byte to be transmitted.