SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
In the idle-line multiprocessor protocol (ADDR/IDLE MODE bit=0), blocks are separated by having a longer idle time between the blocks than between frames in the blocks. An idle time of ten or more high-level bits after a frame indicates the start of a new block. The time of a single bit is calculated directly from the baud value (bits per second). The idle-line multiprocessor communication format is shown in Figure 22-4 (ADDR/IDLE MODE bit is bit 3 of SCICCR).