SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
volatile long int *CSM = (volatile long int *)5F090; //CSM register file volatile
long int *CSMPWL = (volatile long int *)0x78020; //CSM Password location (assuming default Zone select block)
volatile int tmp;
int I;
// Read the 128-bits of the CSM password locations (PWL)
//
for (I=0;I<4; I++) tmp = *CSMPWL++;
// Write the 128-bit password to the CSMKEY registers
// If this password matches that stored in the CSLPWL,
// then the CSM becomes unsecure. If this password does not match,
// then the zone remains secure.
// An example password of: // 0x11112222333344445555666677778888 is used.
*CSM++ = 0x22221111; // Register Z1_CSMKEY0 at 0x5F090
*CSM++ = 0x44443333; // Register Z1_CSMKEY1 at 0x5F092
*CSM++ = 0x66665555; // Register Z1_CSMKEY2 at 0x5F094
*CSM++ = 0x88887777; // Register Z1_CSMKEY3 at 0x5F096