SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The device does not support a swap table for the CLA task vectors (MVECTs). CLA LFU is implemented typically on the CPU side, where the MVECTs are updated sequentially at an appropriate time. The techniques for when to update the MVECTs are described in the LFU system reference design guide, but noted here that the approach is different from the CPU PIE vector table case, where a simple single cycle swap achieves the switch to the new PIE vector table.
For the LS0/LS1 RAM memory swap feature to be useful for CLA LFU switchover, two conditions need to be satisfied: