SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The voltage reference mode must be configured by using either the ADC_setVREF() or the SetVREF() functions, depending on the header files used, provided in C2000Ware. Using either of these functions makes sure that the correct trim is loaded in the ADC trim registers. This function must be called at least once after a device reset. Do not configure the voltage reference mode by directly writing to the ANAREFCTL register.