JAJSS15 November 2023 LMK3H0102
ADVANCE INFORMATION
The internal BAW resonator is divided down by one or two Fractional Output Dividers (FODs). FOD 0 has an SSC generator and FOD 1 does not have an SSC generator. If both OUT0 and OUT1 must be SSC clocks, the two clocks must be sourced by FOD 0. If one SSC clock and one non-SSC clock are required at the same time, then FOD0 is enabled for the SSC clock and FOD1 is enabled for the non-SSC clock. If neither output clock requires SSC, then either FOD can be used.
The maximum frequency that can be generated at the clock outputs by a single FOD is 200 MHz, as the minimum channel divider value is a divide by two. To generate a greater than 200 MHz output, the edge combiner is used, bypassing the channel dividers. This requires that both FODs are enabled and have the same integer divider and fractional numerator values, and the same gain calibration values. When one of the outputs exceeds 200 MHz, the other output can only select the shared FOD frequency divided by one of the channel divider values, or be the FOD frequency. Below 200 MHz, the two FODs can be configured independently so that OUT0 and OUT1 can have different frequencies. TI recommends sourcing from a single FOD whenever possible to make sure that OUT0 and OUT1 have a deterministic phase relationship.
The FODs in the LMK3H0102 can be configured to accommodate various output frequencies through I2C programming, or in the absence of programming, the one-time programmed (OTP) settings. The FODs can be configured by setting the integer (FODx_N_DIV) and fractional (FODx_NUM) divide values. Table 7-5 shows the register locations for these fields for each FOD.
Field | Register |
---|---|
FOD0_N_DIV | R0[9:3] |
FOD0_NUM[23:16] | R1[15:8] |
FOD0_NUM[15:0] | R2[15:0] |
FOD1_N_DIV | R3[15:9] |
FOD1_NUM[23:16] | R6[12:5] |
FOD1_NUM[15:0] | R8[15:0] |
An example of how to set the integer and numerator divide values is shown in Equation 1 and Equation 2.
where:
where FODx_NUM is the fractional portion of the FOD divide value (24 bits, that is 0 to 16777215).
The output frequency (FOUT) is related to the FOD frequency as given in Equation 3, or is equal to the FOD frequency when the edge combiner is enabled. OUTDIV can be 2, 4, 6, 8, 10, 20, or 40.
Use Equation 4 to calculate the actual value of the BAW frequency for a device. Users can find the value of BAWFREQ_OFFSET_FIXEDLUT by reading R238, which is a signed 16-bit value.