SBAA178A March 2011 – November 2026 ADS1286 , ADS7223 , ADS7229 , ADS7230 , ADS7263 , ADS7279 , ADS7280 , ADS774 , ADS7800 , ADS7812 , ADS7813 , ADS7815 , ADS7816 , ADS7817 , ADS7818 , ADS7822 , ADS7822-Q1 , ADS7823 , ADS7824 , ADS7825 , ADS7826 , ADS7827 , ADS7828 , ADS7828-Q1 , ADS7829 , ADS7830 , ADS7834 , ADS7835 , ADS7841 , ADS7841-Q1 , ADS7842 , ADS7844 , ADS7852 , ADS7861 , ADS7862 , ADS7863 , ADS7864 , ADS7865 , ADS7866 , ADS7867 , ADS7868 , ADS7869 , ADS7870 , ADS7871 , ADS7881 , ADS7882 , ADS7883 , ADS7884 , ADS7885 , ADS7886 , ADS7887 , ADS7888 , ADS7890 , ADS7891 , ADS7924 , ADS7945 , ADS7946 , ADS7947 , ADS7948 , ADS7949 , ADS7950 , ADS7951 , ADS7952 , ADS7953 , ADS7954 , ADS7955 , ADS7956 , ADS7957 , ADS7958 , ADS7959 , ADS7960 , ADS7961 , ADS8201 , ADS8284 , ADS8317 , ADS8318 , ADS8319 , ADS8320 , ADS8320-HT , ADS8321 , ADS8322 , ADS8323 , ADS8324 , ADS8325 , ADS8326 , ADS8327 , ADS8328 , ADS8329 , ADS8330 , ADS8331 , ADS8332 , ADS8341 , ADS8342 , ADS8344 , ADS8345 , ADS8361 , ADS8363 , ADS8364 , ADS8365 , ADS8370 , ADS8371 , ADS8372 , ADS8380 , ADS8381 , ADS8382 , ADS8383 , ADS8405 , ADS8406 , ADS8411 , ADS8412 , ADS8413 , ADS8422 , ADS8471 , ADS8472 , ADS8481 , ADS8482 , ADS8484 , ADS8504 , ADS8505 , ADS8506 , ADS8507 , ADS8508 , ADS8509 , ADS8512 , ADS8513 , ADS8515 , ADS8517 , ADS8519 , ADS8528 , ADS8548 , ADS8555 , ADS8556 , ADS8557 , ADS8558 , ADS8568 , ADS8634 , ADS8638 , TLC0820A , TLC0831 , TLC0832 , TLC0834 , TLC0838 , TLC1514 , TLC1518 , TLC1542 , TLC1543 , TLC1543-EP , TLC1549 , TLC1550 , TLC1551 , TLC2543 , TLC2543-EP , TLC2543-Q1 , TLC2543M , TLC2551 , TLC2552 , TLC2554 , TLC2555 , TLC2558 , TLC2574 , TLC2578 , TLC3541 , TLC3544 , TLC3545 , TLC3548 , TLC3574 , TLC3578 , TLC4541 , TLC4545 , TLV0831 , TLV0832 , TLV0834 , TLV0838 , TLV1504 , TLV1508 , TLV1543 , TLV1544 , TLV1548 , TLV1548-EP , TLV1548-Q1 , TLV1548M , TLV1549 , TLV1570 , TLV1571 , TLV1572 , TLV1578 , TLV2541 , TLV2542 , TLV2543 , TLV2544 , TLV2544Q , TLV2545 , TLV2548 , TLV2548-EP , TLV2548M , TLV2548Q , TLV2553 , TLV2553-Q1 , TLV2556 , TLV2556-EP , TLV571
The Laplace transform of voltage V2 in Figure 2-4 is:
where:
The calculations for Equation 1 and Equation 2 are shown in Appendix A. The inverse Laplace transform of Equation 2 is:
After simplifying, Equation 3 can be re-written as follows (see Appendix B for further details):
Equation 5, in turn, can be expressed as:
where time constants
and
are defined as Equation 7 and Equation 8, respectively:
In order to observe the effects of these two time constants, Equation 6 can be rewritten as:
where:
and
The plots of Equation 9, Equation 10, and Equation 11 as a function of time are shown in Figure 3-1.
The following values were used in Figure 3-1: R1 = 100 Ω, R2 = 800 Ω, C1 = 1000 pF, and C2 = 40 pF.
These component values set a =
100 ns, b = 4 ns, and c = 32 ns. These values set ωn =
17.678 Mrad/s and
= 1.202.
Furthermore, the time constants are calculated to be
= 105.721 ns and
= 30.267 ns.
Figure 3-1 Plots of
Equations (8), (9), and (10) versus TimeAs shown in Figure 3-1, k2(t) decays faster than k1(t) when
<<
. Under these conditions,
Equation 9 can be approximated as a function with only time constant
, or: