SLASFM1A June 2025 – December 2025 AFE10004-EP
PRODUCTION DATA
The temperature sensor output is able to be overwritten by externally supplied data. If needed, use this capability to verify the validity of the function stored in the LUT. The externally supplied data act as the temperature sweep input, and the output response caused by temperature is able to be readily observed without altering the temperature of the test setup.
This functionality is facilitated by the multiplexer that follows the temperature sensor, and user-writable temperature overwrite data register (TMPOW[11:0]). The multiplexer control signal is the TMPOW bit. To cancel the temperature sensor overwrite, clear the TMPOW bit.