SLASFM1A June 2025 – December 2025 AFE10004-EP
PRODUCTION DATA
The resistor string structure consists of a series of resistors, each of value R, as shown in Figure 6-2. The code loaded to the DAC determines at which node on the string the voltage is tapped off to be fed into the output amplifier. The voltage is tapped off by closing one of the switches connecting the string to the amplifier. This resistor string architecture has inherent monotonicity, voltage output, and low glitch.
Figure 6-2 DAC Resistor String