To use SYSREF, do the these steps:
- Put the device in SYNC mode using the procedure already outlined.
- Find out IncludedDivide in the same way SYNC mode is done.
- Calculate the SYSREF_DIV_PRE value such that the interpolator frequency
(fINTERPOLATOR) is in the range of 800MHz to 1500MHz.
fINTERPOLATOR = fVCO/IncludedDivide/SYSREF_DIV_PRE.
Make this frequency a multiple of fOSC if possible.
- If using SYSREF generation mode (SYSREF_REPEAT = 0), verify that SysRefReq pin
is high, verify that the SysRefReq pin is high.
- If using SYSREF repeater mode (SYSREF_REPEAT = 1), set up the pulse count if
desired. Pulses are created by toggling the SysRefReq pin.
- Adjust the delay between the RFoutA and RFoutB signal using the JESD_DACx_CTL fields.