STDA033 October 2026 MSPM0G3105-Q1 , MSPM0G3106-Q1 , MSPM0G3107-Q1 , MSPM0G3505-Q1 , MSPM0G3506-Q1 , MSPM0G3507-Q1 , MSPM0L1227-Q1 , MSPM0L1228-Q1 , MSPM0L2227-Q1 , MSPM0L2228-Q1 , MSPM33C321A
If the inductor has a physical core (ferrite, iron powder, and so forth), the inductor also introduces two additional non-ideal behaviors:
Hysteresis Loss: Energy lost as heat when the magnetic domains in the core flip back and forth with the AC signal.
Eddy Current Loss: Small circulating currents induced within the conductive core material, causing further heat.
Magnetic Saturation: While not a "component,"magnetic saturation is a parasitic behavior where the core can no longer hold more magnetic flux. The core eventually reaches a flux level beyond which incremental inductance drops sharply. At this point, the inductance drops sharply, and the rapid current increase can potentially leading to massive current spikes.