SLUUCP8A June 2024 – April 2025 BQ41Z50
This command sets the minimal voltage at the system power converter input at which the system will still operate. This command writes to the data flash value Min System Voltage. It writes it once on the first use to adjust for possible changes in the system design from the time the battery pack was designed.
| SBS Cmd | Name | Access | Protocol | Type | Min | Max | Default | Unit | ||
|---|---|---|---|---|---|---|---|---|---|---|
| SE | US | FA | ||||||||
| 0x5D | TurboEdv() | R/W | R/W | R/W | Word | I2 | 0 | 32767 | mV | |