SNVSC75B April 2023 – September 2025 LM5171-Q1
PRODUCTION DATA
Each channel of the LM5171-Q1 has a bidirectional high accuracy high-speed current sense amplifier. The current sense polarity is determined by the DIR1 and DIR2. The amplifier gain is 40, such that a smaller current sense resistor is supported to reduce power dissipation. The amplified current sense signal is used to perform the following functions:
Select the current sense resistor RCS for 50mV current sense voltage at rated current. Connect the CSA1, CSB1, CSA2 and CSB2 pins via Kelvin connection for accurate sensing.
It is very important that the current sense resistors are low-inductive. Otherwise the sensed current signals are distorted even if the parasitic inductance is only a few nH. Such inductance has only minimal influence on the current regulation during continuous conduction mode, but it affects current zero cross detection, and hence the performance of diode emulation mode under light load. As a consequence, the synchronous rectifier gate pulse is truncated much earlier than the inductor current zero crossing, causing the body diode of the synchronous rectifier to conduct unnecessarily for a longer time. See the Diode Emulation for details.
If the selected current sense resistor has parasitic inductance, see the Section 8.1 for methods to compensate for this condition and achieve optimal performance.